RAIL_ChannelConfigEntry_t Struct Reference

A channel configuration entry structure, which defines a channel range and parameters across which a corresponding radio configuration is valid.

#include < rail_types.h >

Data Fields

const uint32_t * phyConfigDeltaAdd
The minimum radio configuration to apply to the base configuration for this channel set.
uint32_t baseFrequency
A base frequency in Hz of this channel set.
uint32_t channelSpacing
A channel spacing in Hz of this channel set.
uint16_t physicalChannelOffset
The offset to subtract from the logical channel to align them with the zero based physical channels which are relative to baseFrequency.
uint16_t channelNumberStart
The first valid RAIL channel number for this channel set.
uint16_t channelNumberEnd
The last valid RAIL channel number for this channel set.
RAIL_TxPower_t maxPower
The maximum power allowed in this channel set.
RAIL_ChannelConfigEntryAttr_t * attr
A pointer to a structure containing attributes specific to this channel set.
RAIL_ChannelConfigEntryType_t entryType
Indicates channel config type.
uint8_t reserved [3]
to align to 32-bit boundary.

A channel configuration entry structure, which defines a channel range and parameters across which a corresponding radio configuration is valid.

operating frequency = baseFrequency

  • channelSpacing * (channel - physicalChannelOffset);

Definition at line 1616 of file rail_types.h .

Field Documentation

◆ attr

RAIL_ChannelConfigEntryAttr_t * RAIL_ChannelConfigEntry_t::attr

A pointer to a structure containing attributes specific to this channel set.

Definition at line 1632 of file rail_types.h .

◆ baseFrequency

uint32_t RAIL_ChannelConfigEntry_t::baseFrequency

A base frequency in Hz of this channel set.

Definition at line 1619 of file rail_types.h .

◆ channelNumberEnd

uint16_t RAIL_ChannelConfigEntry_t::channelNumberEnd

The last valid RAIL channel number for this channel set.

Definition at line 1629 of file rail_types.h .

◆ channelNumberStart

uint16_t RAIL_ChannelConfigEntry_t::channelNumberStart

The first valid RAIL channel number for this channel set.

Definition at line 1627 of file rail_types.h .

◆ channelSpacing

uint32_t RAIL_ChannelConfigEntry_t::channelSpacing

A channel spacing in Hz of this channel set.

Definition at line 1620 of file rail_types.h .

◆ entryType

RAIL_ChannelConfigEntryType_t RAIL_ChannelConfigEntry_t::entryType

Indicates channel config type.

Definition at line 1635 of file rail_types.h .

◆ maxPower

RAIL_TxPower_t RAIL_ChannelConfigEntry_t::maxPower

The maximum power allowed in this channel set.

Definition at line 1631 of file rail_types.h .

◆ phyConfigDeltaAdd

const uint32_t* RAIL_ChannelConfigEntry_t::phyConfigDeltaAdd

The minimum radio configuration to apply to the base configuration for this channel set.

Definition at line 1617 of file rail_types.h .

◆ physicalChannelOffset

uint16_t RAIL_ChannelConfigEntry_t::physicalChannelOffset

The offset to subtract from the logical channel to align them with the zero based physical channels which are relative to baseFrequency.

(i.e., By default ch 0 = base freq, but if offset = 11, ch 11 = base freq.)

Definition at line 1621 of file rail_types.h .

◆ reserved

uint8_t RAIL_ChannelConfigEntry_t::reserved[3]

to align to 32-bit boundary.

Definition at line 1636 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h