Antenna Diversity Utility
RAIL Antenna Diversity Utility
This optional software component can be enabled to include default functionality related to antenna diversity configuration.
When using a Silicon Labs-developed board, the configuration options for this software component are set up automatically based on the selected board. When using a custom board, manually configure the configuration options.
Configuration Options
The following configuration options can be changed:
- Antenna Diversity:
- Enable/disable receive antenna diversity.
- Enable/disable transmit antenna diversity.
- Enable/disable runtime selection of the receive antenna diversity radio configuration.
The following hardware options can be changed:
- Configure the antenna diversity transmit select GPIO (ANT0 signal).
- Configure the antenna diversity inverse transmit select GPIO (ANT1 signal).