RAILtest Application Graphics
RAILtest Graphics
This software component can optionally be enabled for RAILtest. If enabled, the following information is displayed on the LCD:
- Number of transmitted packets
- Number of received packets
- Channel number
- Application name
When using a Silicon Labs-developed board, the hardware GPIO configuration is set up automatically for this software component based on the selected board. When using a custom board, manually configure the hardware pins. This can be done from within the
Memory LCD
software component. The
Memory LCD
component determines which LCD displays are compatible with the
RAILtest, Graphics
component. (The
Memory LCD
component is a dependency of the
RAILtest, Graphics
component and is included automatically in a project when the
RAILtest, Graphics
component is enabled.)
Configuration Options
The following configuration options can be changed:
-
Alter application name displayed on boot. Default is
RAILtest.