RAIL_DataConfig_t Struct Reference

RAIL data configuration structure.

#include < rail_types.h >

Data Fields

RAIL_TxDataSource_t txSource
Source of TX Data.
RAIL_RxDataSource_t rxSource
Source of RX Data.
RAIL_DataMethod_t txMethod
Method of providing transmit data.
RAIL_DataMethod_t rxMethod
Method of retrieving receive data.

RAIL data configuration structure.

Select the transmit/receive data sources and the method the application uses to provide/retrieve data from RAIL.

Definition at line 2023 of file rail_types.h .

Field Documentation

◆ rxMethod

RAIL_DataMethod_t RAIL_DataConfig_t::rxMethod

Method of retrieving receive data.

Definition at line 2027 of file rail_types.h .

◆ rxSource

RAIL_RxDataSource_t RAIL_DataConfig_t::rxSource

Source of RX Data.

Definition at line 2025 of file rail_types.h .

◆ txMethod

RAIL_DataMethod_t RAIL_DataConfig_t::txMethod

Method of providing transmit data.

Definition at line 2026 of file rail_types.h .

◆ txSource

RAIL_TxDataSource_t RAIL_DataConfig_t::txSource

Source of TX Data.

Definition at line 2024 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h