RAIL_TxChannelHoppingConfigEntry_t Struct Reference

Structure that represents one of the channels that is part of a RAIL_TxChannelHoppingConfig_t sequence of channels used in channel hopping.

#include < rail_types.h >

Data Fields

uint16_t channel
The channel number to be used for this entry in the channel hopping sequence.
uint8_t reserved [2]
Pad bytes reserved for future use and currently ignored.
uint32_t delay
Idle time in microseconds to wait before transmitting on the channel indicated by this entry.

Structure that represents one of the channels that is part of a RAIL_TxChannelHoppingConfig_t sequence of channels used in channel hopping.

Definition at line 2205 of file rail_types.h .

Field Documentation

◆ channel

uint16_t RAIL_TxChannelHoppingConfigEntry_t::channel

The channel number to be used for this entry in the channel hopping sequence.

If this is an invalid channel for the current PHY, the call to RAIL_SetNextTxRepeat() will fail.

Definition at line 2211 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h