Contains arguments for RAIL_BLE_ConfigAox function.

#include < rail_ble.h >

Data Fields

RAIL_BLE_AoxOptions_t aoxOptions
See RAIL_BLE_AOX_OPTIONS_* for bitfield defines for different AoX features.
uint16_t cteBuffSize
Size of the raw AoX CTE (continuous tone extension) data capture buffer in bytes.
uint32_t * cteBuffAddr
Address to where the received CTE is written.
uint8_t * antArrayAddr
Address to first element of antenna pattern array.
uint8_t antArraySize
Size of the antenna pattern array.

Contains arguments for RAIL_BLE_ConfigAox function.

Definition at line 554 of file rail_ble.h .

Field Documentation

◆ antArrayAddr

uint8_t* RAIL_BLE_AoxConfig_t::antArrayAddr

Address to first element of antenna pattern array.

Array must be in RAM. Each element of the array contains an antenna number. The switching pattern is defined by the order of antennas in this array.

Definition at line 573 of file rail_ble.h .


The documentation for this struct was generated from the following file:
  • protocol/ble/ rail_ble.h