Structure for ZCL command "SetMaximumCreditLimit" from "Prepayment".

Public Attributes#

uint32_t

Public Attribute Documentation#

providerId#

uint32_t __zcl_prepayment_cluster_set_maximum_credit_limit_command::providerId

issuerEventId#

uint32_t __zcl_prepayment_cluster_set_maximum_credit_limit_command::issuerEventId

implementationDateTime#

uint32_t __zcl_prepayment_cluster_set_maximum_credit_limit_command::implementationDateTime

maximumCreditLevel#

uint32_t __zcl_prepayment_cluster_set_maximum_credit_limit_command::maximumCreditLevel

maximumCreditPerTopUp#

uint32_t __zcl_prepayment_cluster_set_maximum_credit_limit_command::maximumCreditPerTopUp