EBI - External Bus Interface
Description
EBI External Bus Interface (EBI) Peripheral API.
This module contains functions to control the EBI peripheral of Silicon Labs 32-bit MCUs and SoCs. The EBI is used for accessing external parallel devices. The devices appear as part of the internal memory map of the MCU.
| Data Structures | |
| struct | EBI_Init_TypeDef | 
| EBI Initialization structure. | |
| struct | EBI_TFTInit_TypeDef | 
| TFT Initialization structure. | |
| Functions | |
| void | EBI_Init (const EBI_Init_TypeDef *ebiInit) | 
| Configure and enable the External Bus Interface. | |
| void | EBI_Disable (void) | 
| Disable External Bus Interface. | |
| void | EBI_BankEnable (uint32_t banks, bool enable) | 
| Enable or disable EBI Bank. | |
| uint32_t | EBI_BankAddress (uint32_t bank) | 
| Return the base address of the EBI bank. | |
| void | EBI_NANDFlashEnable (uint32_t banks, bool enable) | 
| Enable or disable EBI NAND Flash Support. | |
| void | EBI_ChipSelectEnable (uint32_t cs, bool enable) | 
| Enable or disable EBI Chip Select. | |
| void | EBI_PolaritySet ( EBI_Line_TypeDef line, EBI_Polarity_TypeDef polarity) | 
| Configure EBI pin polarity. | |
| void | EBI_ReadTimingSet (uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles) | 
| Configure timing values of read bus accesses. | |
| void | EBI_WriteTimingSet (uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles) | 
| Configure timing values of write bus accesses. | |
| void | EBI_AddressTimingSet (uint32_t setupCycles, uint32_t holdCycles) | 
| Configure timing values of address latch bus accesses. | |
| void | EBI_TFTInit (const EBI_TFTInit_TypeDef *ebiTFTInit) | 
| Configure and initialize TFT Direct Drive. | |
| void | EBI_TFTSizeSet (uint32_t horizontal, uint32_t vertical) | 
| Configure and initialize TFT size settings. | |
| void | EBI_TFTHPorchSet (uint32_t front, uint32_t back, uint32_t pulseWidth) | 
| Configure and initialize Horizontal Porch Settings. | |
| void | EBI_TFTVPorchSet (uint32_t front, uint32_t back, uint32_t pulseWidth) | 
| Configure Vertical Porch Settings. | |
| void | EBI_TFTTimingSet (uint32_t dclkPeriod, uint32_t start, uint32_t setup, uint32_t hold) | 
| Configure TFT Direct Drive Timing Settings. | |
| void | EBI_BankReadTimingConfig (uint32_t banks, bool pageMode, bool prefetch, bool halfRE) | 
| Configure read operation parameters for a selected bank. | |
| void | EBI_BankReadTimingSet (uint32_t banks, uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles) | 
| Configure timing values of read bus accesses. | |
| void | EBI_BankWriteTimingConfig (uint32_t banks, bool writeBufDisable, bool halfWE) | 
| Configure write operation parameters for a selected bank. | |
| void | EBI_BankWriteTimingSet (uint32_t banks, uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles) | 
| Configure timing values of write bus accesses. | |
| void | EBI_BankAddressTimingConfig (uint32_t banks, bool halfALE) | 
| Configure address operation parameters for a selected bank. | |
| void | EBI_BankAddressTimingSet (uint32_t banks, uint32_t setupCycles, uint32_t holdCycles) | 
| Configure timing values of address latch bus accesses. | |
| void | EBI_BankPolaritySet (uint32_t banks, EBI_Line_TypeDef line, EBI_Polarity_TypeDef polarity) | 
| Configure EBI pin polarity for selected bank(s) for devices with individual timing support. | |
| void | EBI_BankByteLaneEnable (uint32_t banks, bool enable) | 
| Configure Byte Lane Enable for select banks timing support. | |
| void | EBI_AltMapEnable (bool enable) | 
| Configure the Alternate Address Map support. | |
| void | EBI_TFTEnable ( EBI_TFTDDMode_TypeDef mode) | 
| Enable or disable TFT Direct Drive. | |
| void | EBI_TFTFrameBaseSet (uint32_t address) | 
| Configure frame buffer pointer. | |
| void | EBI_TFTPixelSet (int pixel, uint32_t color) | 
| Set TFT Pixel Color 0 or 1. | |
| void | EBI_TFTDDSet (uint32_t color) | 
| Set TFT Direct Drive Data from Internal Memory. | |
| void | EBI_TFTColorFormatSet ( EBI_TFTColorFormat_TypeDef color0, EBI_TFTColorFormat_TypeDef color1) | 
| Set TFT Color Format. | |
| void | EBI_TFTMaskBlendMode ( EBI_TFTMaskBlend_TypeDef maskBlend) | 
| Masking and Blending Mode Set. | |
| void | EBI_TFTColorSrcSet ( EBI_TFTColorSrc_TypeDef colorSrc) | 
| Masking and Blending Color1 Source Set. | |
| void | EBI_TFTAlphaBlendSet (uint8_t alpha) | 
| Set TFT Alpha Blending Factor. | |
| void | EBI_TFTMaskSet (uint32_t mask) | 
| Set TFT mask value. | |
| uint32_t | EBI_TFTVCount (void) | 
| Get current vertical position counter. | |
| uint32_t | EBI_TFTHCount (void) | 
| Get current horizontal position counter. | |
| void | EBI_TFTFBTriggerSet ( EBI_TFTFrameBufTrigger_TypeDef sync) | 
| Set Frame Buffer Trigger. | |
| void | EBI_TFTHStrideSet (uint32_t nbytes) | 
| Set horizontal TFT stride value in number of bytes. | |
| void | EBI_IntClear (uint32_t flags) | 
| Clear one or more pending EBI interrupts. | |
| void | EBI_IntSet (uint32_t flags) | 
| Set one or more pending EBI interrupts. | |
| void | EBI_IntDisable (uint32_t flags) | 
| Disable one or more EBI interrupts. | |
| void | EBI_IntEnable (uint32_t flags) | 
| Enable one or more EBI interrupts. | |
| uint32_t | EBI_IntGet (void) | 
| Get pending EBI interrupt flags. | |
| uint32_t | EBI_IntGetEnabled (void) | 
| Get enabled and pending EBI interrupt flags. | |
| void | EBI_StartNandEccGen (void) | 
| Start ECC generator on NAND flash transfers. | |
| uint32_t | EBI_StopNandEccGen (void) | 
| Stop NAND flash ECC generator and return generated ECC. | |
| Macros | |
| #define | EBI_BANK0 (uint32_t)(1 << 1) | 
| EBI address bank 0. | |
| #define | EBI_BANK1 (uint32_t)(1 << 2) | 
| EBI address bank 1. | |
| #define | EBI_BANK2 (uint32_t)(1 << 3) | 
| EBI address bank 2. | |
| #define | EBI_BANK3 (uint32_t)(1 << 4) | 
| EBI address bank 3. | |
| #define | EBI_CS0 (uint32_t)(1 << 1) | 
| EBI chip select line 0. | |
| #define | EBI_CS1 (uint32_t)(1 << 2) | 
| EBI chip select line 1. | |
| #define | EBI_CS2 (uint32_t)(1 << 3) | 
| EBI chip select line 2. | |
| #define | EBI_CS3 (uint32_t)(1 << 4) | 
| EBI chip select line 3. | |
| #define | EBI_GENERIC_ALB_A0 EBI_ROUTEPEN_ALB_A0 | 
| Pin Enable Lower Bound EBI_A[0] and upwards. | |
| #define | EBI_GENERIC_ALB_A8 EBI_ROUTEPEN_ALB_A8 | 
| Pin Enable Lower Bound EBI_A[8] and upwards. | |
| #define | EBI_GENERIC_ALB_A16 EBI_ROUTEPEN_ALB_A16 | 
| Pin Enable Lower Bound EBI_A[16] and upwards. | |
| #define | EBI_GENERIC_ALB_A24 EBI_ROUTEPEN_ALB_A24 | 
| Pin Enable Lower Bound EBI_A[24] and upwards. | |
| #define | EBI_GENERIC_APEN_A0 EBI_ROUTEPEN_APEN_A0 | 
| All EBI_A pins enabled. | |
| #define | EBI_GENERIC_APEN_A5 EBI_ROUTEPEN_APEN_A5 | 
| EBI_A[4:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A6 EBI_ROUTEPEN_APEN_A6 | 
| EBI_A[5:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A7 EBI_ROUTEPEN_APEN_A7 | 
| EBI_A[6:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A8 EBI_ROUTEPEN_APEN_A8 | 
| EBI_A[7:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A9 EBI_ROUTEPEN_APEN_A9 | 
| EBI_A[8:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A10 EBI_ROUTEPEN_APEN_A10 | 
| EBI_A[9:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A11 EBI_ROUTEPEN_APEN_A11 | 
| EBI_A[10:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A12 EBI_ROUTEPEN_APEN_A12 | 
| EBI_A[11:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A13 EBI_ROUTEPEN_APEN_A13 | 
| EBI_A[12:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A14 EBI_ROUTEPEN_APEN_A14 | 
| EBI_A[13:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A15 EBI_ROUTEPEN_APEN_A15 | 
| EBI_A[14:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A16 EBI_ROUTEPEN_APEN_A16 | 
| EBI_A[15:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A17 EBI_ROUTEPEN_APEN_A17 | 
| EBI_A[16:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A18 EBI_ROUTEPEN_APEN_A18 | 
| EBI_A[17:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A19 EBI_ROUTEPEN_APEN_A19 | 
| EBI_A[18:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A20 EBI_ROUTEPEN_APEN_A20 | 
| EBI_A[19:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A21 EBI_ROUTEPEN_APEN_A21 | 
| EBI_A[20:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A22 EBI_ROUTEPEN_APEN_A22 | 
| EBI_A[21:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A23 EBI_ROUTEPEN_APEN_A23 | 
| EBI_A[22:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A24 EBI_ROUTEPEN_APEN_A24 | 
| EBI_A[23:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A25 EBI_ROUTEPEN_APEN_A25 | 
| EBI_A[24:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A26 EBI_ROUTEPEN_APEN_A26 | 
| EBI_A[25:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A27 EBI_ROUTEPEN_APEN_A27 | 
| EBI_A[26:L] pins enabled. | |
| #define | EBI_GENERIC_APEN_A28 EBI_ROUTEPEN_APEN_A28 | 
| EBI_A[27:L] pins enabled. | |
| #define | EBI_INIT_DEFAULT | 
| Default configuration for EBI initialization structures. | |
| #define | EBI_TFTINIT_DEFAULT | 
| Default configuration for EBI TFT initialization structure. | |
| Enumerations | |
| enum | EBI_Mode_TypeDef
         
         { ebiModeD8A8 = EBI_CTRL_MODE_D8A8, ebiModeD16A16ALE = EBI_CTRL_MODE_D16A16ALE, ebiModeD8A24ALE = EBI_CTRL_MODE_D8A24ALE, ebiModeD16 = EBI_CTRL_MODE_D16 } | 
| EBI Mode of operation. | |
| enum | EBI_Polarity_TypeDef
         
         { ebiActiveLow = 0, ebiActiveHigh = 1 } | 
| EBI Polarity configuration. | |
| enum | EBI_Line_TypeDef
         
         { ebiLineARDY , ebiLineALE , ebiLineWE , ebiLineRE , ebiLineCS , ebiLineBL , ebiLineTFTVSync , ebiLineTFTHSync , ebiLineTFTDataEn , ebiLineTFTDClk , ebiLineTFTCS } | 
| EBI Pin Line types. | |
| enum | EBI_ALow_TypeDef
         
         { ebiALowA0 = EBI_GENERIC_ALB_A0, ebiALowA8 = EBI_GENERIC_ALB_A8, ebiALowA16 = EBI_GENERIC_ALB_A16, ebiALowA24 = EBI_GENERIC_ALB_A24 } | 
| Address Pin Enable, lower limit - lower range of pins to enable. | |
| enum | EBI_AHigh_TypeDef
         
         { ebiAHighA0 = EBI_GENERIC_APEN_A0, ebiAHighA5 = EBI_GENERIC_APEN_A5, ebiAHighA6 = EBI_GENERIC_APEN_A6, ebiAHighA7 = EBI_GENERIC_APEN_A7, ebiAHighA8 = EBI_GENERIC_APEN_A8, ebiAHighA9 = EBI_GENERIC_APEN_A9, ebiAHighA10 = EBI_GENERIC_APEN_A10, ebiAHighA11 = EBI_GENERIC_APEN_A11, ebiAHighA12 = EBI_GENERIC_APEN_A12, ebiAHighA13 = EBI_GENERIC_APEN_A13, ebiAHighA14 = EBI_GENERIC_APEN_A14, ebiAHighA15 = EBI_GENERIC_APEN_A15, ebiAHighA16 = EBI_GENERIC_APEN_A16, ebiAHighA17 = EBI_GENERIC_APEN_A17, ebiAHighA18 = EBI_GENERIC_APEN_A18, ebiAHighA19 = EBI_GENERIC_APEN_A19, ebiAHighA20 = EBI_GENERIC_APEN_A20, ebiAHighA21 = EBI_GENERIC_APEN_A21, ebiAHighA22 = EBI_GENERIC_APEN_A22, ebiAHighA23 = EBI_GENERIC_APEN_A23, ebiAHighA24 = EBI_GENERIC_APEN_A24, ebiAHighA25 = EBI_GENERIC_APEN_A25, ebiAHighA26 = EBI_GENERIC_APEN_A26, ebiAHighA27 = EBI_GENERIC_APEN_A27, ebiAHighA28 = EBI_GENERIC_APEN_A28 } | 
| Address Pin Enable, high limit - higher limit of pins to enable. | |
| enum | EBI_TFTBank_TypeDef
         
         { ebiTFTBank0 = EBI_TFTCTRL_BANKSEL_BANK0, ebiTFTBank1 = EBI_TFTCTRL_BANKSEL_BANK1, ebiTFTBank2 = EBI_TFTCTRL_BANKSEL_BANK2, ebiTFTBank3 = EBI_TFTCTRL_BANKSEL_BANK3 } | 
| EBI TFT Graphics Bank Select. | |
| enum | EBI_TFTColorFormat_TypeDef
         
         { ebiTFTARGB0555 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0555, ebiTFTARGB0565 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0565, ebiTFTARGB0666 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0666, ebiTFTARGB0888 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0888, ebiTFTARGB5555 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB5555, ebiTFTARGB6565 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB6565, ebiTFTARGB6666 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB6666, ebiTFTARGB8888 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB8888, ebiTFTRGB555 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB555, ebiTFTRGB565 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB565, ebiTFTRGB666 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB666, ebiTFTRGB888 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB888 } | 
| EBI TFT Color format. | |
| enum | EBI_TFTColorSrc_TypeDef
         
         { ebiTFTColorSrcMem = EBI_TFTCTRL_COLOR1SRC_MEM, ebiTFTColorSrcPixel1 = EBI_TFTCTRL_COLOR1SRC_PIXEL1 } | 
| Masking and Alpha blending source color. | |
| enum | EBI_TFTInterleave_TypeDef
         
         { ebiTFTInterleaveUnlimited = EBI_TFTCTRL_INTERLEAVE_UNLIMITED, ebiTFTInterleaveOnePerDClk = EBI_TFTCTRL_INTERLEAVE_ONEPERDCLK, ebiTFTInterleavePorch = EBI_TFTCTRL_INTERLEAVE_PORCH } | 
| Bus Data Interleave Mode. | |
| enum | EBI_TFTFrameBufTrigger_TypeDef
         
         { ebiTFTFrameBufTriggerVSync = EBI_TFTCTRL_FBCTRIG_VSYNC, ebiTFTFrameBufTriggerHSync = EBI_TFTCTRL_FBCTRIG_HSYNC } | 
| Control frame base pointer copy. | |
| enum | EBI_TFTMaskBlend_TypeDef
         
         { ebiTFTMBDisabled = EBI_TFTCTRL_MASKBLEND_DISABLED, ebiTFTMBIMask = EBI_TFTCTRL_MASKBLEND_IMASK, ebiTFTMBIAlpha = EBI_TFTCTRL_MASKBLEND_IALPHA, ebiTFTMBIMaskAlpha = EBI_TFTCTRL_MASKBLEND_IMASKALPHA, ebiTFTMBEMask = EBI_TFTCTRL_MASKBLEND_EFBMASK, ebiTFTMBEAlpha = EBI_TFTCTRL_MASKBLEND_EFBALPHA, ebiTFTMBEMaskAlpha = EBI_TFTCTRL_MASKBLEND_EFBMASKALPHA, ebiTFTMBEIMask = EBI_TFTCTRL_MASKBLEND_IFBMASK, ebiTFTMBEIAlpha = EBI_TFTCTRL_MASKBLEND_IFBALPHA, ebiTFTMBEIMaskAlpha = EBI_TFTCTRL_MASKBLEND_IFBMASKALPHA } | 
| Control of mask and alpha blending mode. | |
| enum | EBI_TFTDDMode_TypeDef
         
         { ebiTFTDDModeDisabled = EBI_TFTCTRL_DD_DISABLED, ebiTFTDDModeInternal = EBI_TFTCTRL_DD_INTERNAL, ebiTFTDDModeExternal = EBI_TFTCTRL_DD_EXTERNAL } | 
| TFT Direct Drive mode. | |
| enum | EBI_TFTWidth_TypeDef
         
         { ebiTFTWidthByte = EBI_TFTCTRL_WIDTH_BYTE, ebiTFTWidthHalfWord = EBI_TFTCTRL_WIDTH_HALFWORD } | 
| TFT Data Increment Width. | |
Function Documentation
◆ EBI_Init()
| void EBI_Init | ( | const EBI_Init_TypeDef * | 
            ebiInit
            | ) | 
Configure and enable the External Bus Interface.
- Parameters
- 
         [in] ebiInitThe EBI configuration structure. 
- Note
- GPIO lines must be configured as a PUSH_PULL for the correct operation. GPIO and EBI clocks must be enabled in the CMU.
◆ EBI_Disable()
| void EBI_Disable | ( | void | 
            | ) | 
Disable External Bus Interface.
◆ EBI_BankEnable()
| void EBI_BankEnable | ( | uint32_t | 
            banks,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable or disable EBI Bank.
- Parameters
- 
         [in] banksBanks to reconfigure, mask of EBI_BANK<n> flags. [in] enableTrue to enable, false to disable. 
◆ EBI_BankAddress()
| uint32_t EBI_BankAddress | ( | uint32_t | 
            bank
            | ) | 
Return the base address of the EBI bank.
- Parameters
- 
         [in] bankA bank to return the start address for. 
- Returns
- an absolute address of the bank.
◆ EBI_NANDFlashEnable()
| void EBI_NANDFlashEnable | ( | uint32_t | 
            banks,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable or disable EBI NAND Flash Support.
- Parameters
- 
         [in] banksBanks to reconfigure, mask of EBI_BANK<n> flags. [in] enableTrue to enable, false to disable. 
◆ EBI_ChipSelectEnable()
| void EBI_ChipSelectEnable | ( | uint32_t | 
            cs,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable or disable EBI Chip Select.
- Parameters
- 
         [in] csChipSelect lines to reconfigure, mask of EBI_CS<n> flags. [in] enableTrue to enable, false to disable. 
◆ EBI_PolaritySet()
| void EBI_PolaritySet | ( | EBI_Line_TypeDef | 
            line,
            | 
| EBI_Polarity_TypeDef | 
            polarity
            | ||
| ) | 
Configure EBI pin polarity.
- Parameters
- 
         [in] lineWhich pin/line to configure. [in] polarityActive high or active low. 
◆ EBI_ReadTimingSet()
| void EBI_ReadTimingSet | ( | uint32_t | 
            setupCycles,
            | 
| uint32_t | 
            strobeCycles,
            | ||
| uint32_t | 
            holdCycles
            | ||
| ) | 
Configure timing values of read bus accesses.
- Parameters
- 
         [in] setupCyclesA number of clock cycles for the address setup before REn is asserted. [in] strobeCyclesThe number of cycles the REn is held active. After the specified number of cycles, data is read. If set to 0, 1 cycle is inserted by hardware. [in] holdCyclesThe number of cycles CSn is held active after the REn is deasserted. 
◆ EBI_WriteTimingSet()
| void EBI_WriteTimingSet | ( | uint32_t | 
            setupCycles,
            | 
| uint32_t | 
            strobeCycles,
            | ||
| uint32_t | 
            holdCycles
            | ||
| ) | 
Configure timing values of write bus accesses.
- Parameters
- 
         [in] setupCyclesA number of clock cycles for the address setup before WEn is asserted. [in] strobeCyclesA number of cycles WEn is held active. If set to 0, 1 cycle is inserted by hardware. [in] holdCyclesA number of cycles CSn is held active after the WEn is deasserted. 
◆ EBI_AddressTimingSet()
| void EBI_AddressTimingSet | ( | uint32_t | 
            setupCycles,
            | 
| uint32_t | 
            holdCycles
            | ||
| ) | 
Configure timing values of address latch bus accesses.
- Parameters
- 
         [in] setupCyclesSets the number of cycles the address is held after ALE is asserted. [in] holdCyclesSets the number of cycles the address is driven onto the ADDRDAT bus before ALE is asserted. If set 0, 1 cycle is inserted by hardware. 
◆ EBI_TFTInit()
| void EBI_TFTInit | ( | const EBI_TFTInit_TypeDef * | 
            ebiTFTInit
            | ) | 
Configure and initialize TFT Direct Drive.
- Parameters
- 
         [in] ebiTFTInitThe TFT Initialization structure. 
◆ EBI_TFTSizeSet()
| void EBI_TFTSizeSet | ( | uint32_t | 
            horizontal,
            | 
| uint32_t | 
            vertical
            | ||
| ) | 
Configure and initialize TFT size settings.
- Parameters
- 
         [in] horizontalTFT display horizontal size in pixels. [in] verticalTFT display vertical size in pixels. 
◆ EBI_TFTHPorchSet()
| void EBI_TFTHPorchSet | ( | uint32_t | 
            front,
            | 
| uint32_t | 
            back,
            | ||
| uint32_t | 
            pulseWidth
            | ||
| ) | 
Configure and initialize Horizontal Porch Settings.
- Parameters
- 
         [in] frontHorizontal front porch size in pixels. [in] backHorizontal back porch size in pixels. [in] pulseWidthHorizontal synchronization pulse width. Set to required -1. 
◆ EBI_TFTVPorchSet()
| void EBI_TFTVPorchSet | ( | uint32_t | 
            front,
            | 
| uint32_t | 
            back,
            | ||
| uint32_t | 
            pulseWidth
            | ||
| ) | 
Configure Vertical Porch Settings.
- Parameters
- 
         [in] frontVertical front porch size in pixels. [in] backVertical back porch size in pixels. [in] pulseWidthVertical synchronization pulse width. Set to required -1. 
◆ EBI_TFTTimingSet()
| void EBI_TFTTimingSet | ( | uint32_t | 
            dclkPeriod,
            | 
| uint32_t | 
            start,
            | ||
| uint32_t | 
            setup,
            | ||
| uint32_t | 
            hold
            | ||
| ) | 
Configure TFT Direct Drive Timing Settings.
- Parameters
- 
         [in] dclkPeriodDCLK period in internal cycles. [in] startA starting position of the external direct drive, relative to the DCLK inactive edge. [in] setupA number of cycles that RGB data is driven before the active edge of DCLK. [in] holdA number of cycles that RGB data is held after the active edge of DCLK. 
◆ EBI_BankReadTimingConfig()
| void EBI_BankReadTimingConfig | ( | uint32_t | 
            banks,
            | 
| bool | 
            pageMode,
            | ||
| bool | 
            prefetch,
            | ||
| bool | 
            halfRE
            | ||
| ) | 
Configure read operation parameters for a selected bank.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure write timing for. [in] pageModeEnables or disables the half cycle WE strobe in the last strobe cycle. [in] prefetchEnables or disables the half cycle WE strobe in the last strobe cycle. [in] halfREEnables or disables the half cycle WE strobe in the last strobe cycle. 
◆ EBI_BankReadTimingSet()
| void EBI_BankReadTimingSet | ( | uint32_t | 
            banks,
            | 
| uint32_t | 
            setupCycles,
            | ||
| uint32_t | 
            strobeCycles,
            | ||
| uint32_t | 
            holdCycles
            | ||
| ) | 
Configure timing values of read bus accesses.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure timing for. [in] setupCyclesA number of clock cycles for address setup before REn is asserted. [in] strobeCyclesThe number of cycles the REn is held active. After the specified number of cycles, data is read. If set to 0, 1 cycle is inserted by hardware. [in] holdCyclesThe number of cycles CSn is held active after the REn is deasserted. 
◆ EBI_BankWriteTimingConfig()
| void EBI_BankWriteTimingConfig | ( | uint32_t | 
            banks,
            | 
| bool | 
            writeBufDisable,
            | ||
| bool | 
            halfWE
            | ||
| ) | 
Configure write operation parameters for a selected bank.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure write timing for. [in] writeBufDisableIf true, disable the write buffer. [in] halfWEEnables or disables half cycle WE strobe in the last strobe cycle. 
◆ EBI_BankWriteTimingSet()
| void EBI_BankWriteTimingSet | ( | uint32_t | 
            banks,
            | 
| uint32_t | 
            setupCycles,
            | ||
| uint32_t | 
            strobeCycles,
            | ||
| uint32_t | 
            holdCycles
            | ||
| ) | 
Configure timing values of write bus accesses.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure write timing for. [in] setupCyclesA number of clock cycles for address setup before WEn is asserted. [in] strobeCyclesA number of cycles WEn is held active. If set to 0, 1 cycle is inserted by hardware. [in] holdCyclesNumber of cycles CSn is held active after WEn is deasserted. 
◆ EBI_BankAddressTimingConfig()
| void EBI_BankAddressTimingConfig | ( | uint32_t | 
            banks,
            | 
| bool | 
            halfALE
            | ||
| ) | 
Configure address operation parameters for a selected bank.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure write timing for. [in] halfALEEnables or disables the half cycle ALE strobe in the last strobe cycle. 
◆ EBI_BankAddressTimingSet()
| void EBI_BankAddressTimingSet | ( | uint32_t | 
            banks,
            | 
| uint32_t | 
            setupCycles,
            | ||
| uint32_t | 
            holdCycles
            | ||
| ) | 
Configure timing values of address latch bus accesses.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure address timing for. [in] setupCyclesSets the number of cycles the address is held after ALE is asserted. [in] holdCyclesSets the number of cycles the address is driven onto the ADDRDAT bus before ALE is asserted. If set 0, 1 cycle is inserted by hardware. 
◆ EBI_BankPolaritySet()
| void EBI_BankPolaritySet | ( | uint32_t | 
            banks,
            | 
| EBI_Line_TypeDef | 
            line,
            | ||
| EBI_Polarity_TypeDef | 
            polarity
            | ||
| ) | 
Configure EBI pin polarity for selected bank(s) for devices with individual timing support.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure polarity for. [in] lineWhich pin/line to configure. [in] polarityActive high, or active low. 
◆ EBI_BankByteLaneEnable()
| void EBI_BankByteLaneEnable | ( | uint32_t | 
            banks,
            | 
| bool | 
            enable
            | ||
| ) | 
Configure Byte Lane Enable for select banks timing support.
- Parameters
- 
         [in] banksA mask of memory bank(s) to configure polarity for. [in] enableA flag 
◆ EBI_AltMapEnable()
| void EBI_AltMapEnable | ( | bool | 
            enable
            | ) | 
Configure the Alternate Address Map support.
Enables or disables 256 MB address range for all banks.
- Parameters
- 
         [in] enableSet or clear the address map extension. 
◆ EBI_TFTEnable()
| 
 | inline | 
Enable or disable TFT Direct Drive.
- Parameters
- 
         [in] modeDrive from Internal or External memory, or Disable Direct Drive. 
◆ EBI_TFTFrameBaseSet()
| 
 | inline | 
Configure frame buffer pointer.
- Parameters
- 
         [in] addressFrame pointer address, as offset by EBI base address. 
◆ EBI_TFTPixelSet()
| 
 | inline | 
Set TFT Pixel Color 0 or 1.
- Parameters
- 
         [in] pixelWhich pixel instance to set. [in] colorColor of pixel, 16-bit value. 
◆ EBI_TFTDDSet()
| 
 | inline | 
Set TFT Direct Drive Data from Internal Memory.
- Parameters
- 
         [in] colorColor of pixel 
◆ EBI_TFTColorFormatSet()
| 
 | inline | 
Set TFT Color Format.
- Parameters
- 
         [in] color0ARGB color format to be used. [in] color1RGB color format to be used. 
◆ EBI_TFTMaskBlendMode()
| 
 | inline | 
Masking and Blending Mode Set.
- Parameters
- 
         [in] maskBlendMasking and alpha blending mode. 
◆ EBI_TFTColorSrcSet()
| 
 | inline | 
Masking and Blending Color1 Source Set.
- Parameters
- 
         [in] colorSrcColor1 source. 
◆ EBI_TFTAlphaBlendSet()
| 
 | inline | 
Set TFT Alpha Blending Factor.
- Parameters
- 
         [in] alpha8-bit value indicating blending factor. 
◆ EBI_TFTMaskSet()
| 
 | inline | 
Set TFT mask value.
Data accesses that matches this value are suppressed.
- Parameters
- 
         [in] mask
◆ EBI_TFTVCount()
| 
 | inline | 
Get current vertical position counter.
- Returns
- Returns the current line position for the visible part of a frame.
◆ EBI_TFTHCount()
| 
 | inline | 
Get current horizontal position counter.
- Returns
- Returns the current horizontal pixel position within a visible line.
◆ EBI_TFTFBTriggerSet()
| 
 | inline | 
Set Frame Buffer Trigger.
Frame buffer pointer will be updated either on each horizontal line (hsync) or vertical update (vsync).
- Parameters
- 
         [in] syncTrigger update of frame buffer pointer on vertical or horizontal sync. 
◆ EBI_TFTHStrideSet()
| 
 | inline | 
Set horizontal TFT stride value in number of bytes.
- Parameters
- 
         [in] nbytesNumber of bytes to add to frame buffer pointer after each horizontal line update. 
◆ EBI_IntClear()
| 
 | inline | 
Clear one or more pending EBI interrupts.
- Parameters
- 
         [in] flagsPending EBI interrupt source to clear. Use a logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn). 
◆ EBI_IntSet()
| 
 | inline | 
Set one or more pending EBI interrupts.
- Parameters
- 
         [in] flagsEBI interrupt sources to set to pending. Use a logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn). 
◆ EBI_IntDisable()
| 
 | inline | 
Disable one or more EBI interrupts.
- Parameters
- 
         [in] flagsEBI interrupt sources to disable. Use logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn) 
◆ EBI_IntEnable()
| 
 | inline | 
Enable one or more EBI interrupts.
- Parameters
- 
         [in] flagsEBI interrupt sources to enable. Use logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn) 
◆ EBI_IntGet()
| 
 | inline | 
Get pending EBI interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Returns
- EBI interrupt sources pending, a logical combination of valid EBI interrupt flags, EBI_IF_nnn.
◆ EBI_IntGetEnabled()
| 
 | inline | 
Get enabled and pending EBI interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- 
         Pending and enabled EBI interrupt sources. The return value is the bitwise AND of
         - the enabled interrupt sources in EBI_IEN and
- the pending interrupt flags EBI_IF.
 
◆ EBI_StartNandEccGen()
| 
 | inline | 
Start ECC generator on NAND flash transfers.
◆ EBI_StopNandEccGen()
| 
 | inline | 
Stop NAND flash ECC generator and return generated ECC.
- Returns
- The generated ECC.
Macro Definition Documentation
◆ EBI_BANK0
| #define EBI_BANK0 (uint32_t)(1 << 1) | 
EBI address bank 0.
* * --------- --------- * | | /| |\ | Ext. | * | EBI | / --------- \ | Async | * | | \ --------- / | Device| * | | \| |/ | | * --------- --------- * Parallel interface * *
◆ EBI_BANK1
| #define EBI_BANK1 (uint32_t)(1 << 2) | 
EBI address bank 1.
◆ EBI_BANK2
| #define EBI_BANK2 (uint32_t)(1 << 3) | 
EBI address bank 2.
◆ EBI_BANK3
| #define EBI_BANK3 (uint32_t)(1 << 4) | 
EBI address bank 3.
◆ EBI_CS0
| #define EBI_CS0 (uint32_t)(1 << 1) | 
EBI chip select line 0.
◆ EBI_CS1
| #define EBI_CS1 (uint32_t)(1 << 2) | 
EBI chip select line 1.
◆ EBI_CS2
| #define EBI_CS2 (uint32_t)(1 << 3) | 
EBI chip select line 2.
◆ EBI_CS3
| #define EBI_CS3 (uint32_t)(1 << 4) | 
EBI chip select line 3.
◆ EBI_GENERIC_ALB_A0
| #define EBI_GENERIC_ALB_A0 EBI_ROUTEPEN_ALB_A0 | 
Pin Enable Lower Bound EBI_A[0] and upwards.
◆ EBI_GENERIC_ALB_A8
| #define EBI_GENERIC_ALB_A8 EBI_ROUTEPEN_ALB_A8 | 
Pin Enable Lower Bound EBI_A[8] and upwards.
◆ EBI_GENERIC_ALB_A16
| #define EBI_GENERIC_ALB_A16 EBI_ROUTEPEN_ALB_A16 | 
Pin Enable Lower Bound EBI_A[16] and upwards.
◆ EBI_GENERIC_ALB_A24
| #define EBI_GENERIC_ALB_A24 EBI_ROUTEPEN_ALB_A24 | 
Pin Enable Lower Bound EBI_A[24] and upwards.
◆ EBI_GENERIC_APEN_A0
| #define EBI_GENERIC_APEN_A0 EBI_ROUTEPEN_APEN_A0 | 
All EBI_A pins enabled.
◆ EBI_GENERIC_APEN_A5
| #define EBI_GENERIC_APEN_A5 EBI_ROUTEPEN_APEN_A5 | 
EBI_A[4:L] pins enabled.
◆ EBI_GENERIC_APEN_A6
| #define EBI_GENERIC_APEN_A6 EBI_ROUTEPEN_APEN_A6 | 
EBI_A[5:L] pins enabled.
◆ EBI_GENERIC_APEN_A7
| #define EBI_GENERIC_APEN_A7 EBI_ROUTEPEN_APEN_A7 | 
EBI_A[6:L] pins enabled.
◆ EBI_GENERIC_APEN_A8
| #define EBI_GENERIC_APEN_A8 EBI_ROUTEPEN_APEN_A8 | 
EBI_A[7:L] pins enabled.
◆ EBI_GENERIC_APEN_A9
| #define EBI_GENERIC_APEN_A9 EBI_ROUTEPEN_APEN_A9 | 
EBI_A[8:L] pins enabled.
◆ EBI_GENERIC_APEN_A10
| #define EBI_GENERIC_APEN_A10 EBI_ROUTEPEN_APEN_A10 | 
EBI_A[9:L] pins enabled.
◆ EBI_GENERIC_APEN_A11
| #define EBI_GENERIC_APEN_A11 EBI_ROUTEPEN_APEN_A11 | 
EBI_A[10:L] pins enabled.
◆ EBI_GENERIC_APEN_A12
| #define EBI_GENERIC_APEN_A12 EBI_ROUTEPEN_APEN_A12 | 
EBI_A[11:L] pins enabled.
◆ EBI_GENERIC_APEN_A13
| #define EBI_GENERIC_APEN_A13 EBI_ROUTEPEN_APEN_A13 | 
EBI_A[12:L] pins enabled.
◆ EBI_GENERIC_APEN_A14
| #define EBI_GENERIC_APEN_A14 EBI_ROUTEPEN_APEN_A14 | 
EBI_A[13:L] pins enabled.
◆ EBI_GENERIC_APEN_A15
| #define EBI_GENERIC_APEN_A15 EBI_ROUTEPEN_APEN_A15 | 
EBI_A[14:L] pins enabled.
◆ EBI_GENERIC_APEN_A16
| #define EBI_GENERIC_APEN_A16 EBI_ROUTEPEN_APEN_A16 | 
EBI_A[15:L] pins enabled.
◆ EBI_GENERIC_APEN_A17
| #define EBI_GENERIC_APEN_A17 EBI_ROUTEPEN_APEN_A17 | 
EBI_A[16:L] pins enabled.
◆ EBI_GENERIC_APEN_A18
| #define EBI_GENERIC_APEN_A18 EBI_ROUTEPEN_APEN_A18 | 
EBI_A[17:L] pins enabled.
◆ EBI_GENERIC_APEN_A19
| #define EBI_GENERIC_APEN_A19 EBI_ROUTEPEN_APEN_A19 | 
EBI_A[18:L] pins enabled.
◆ EBI_GENERIC_APEN_A20
| #define EBI_GENERIC_APEN_A20 EBI_ROUTEPEN_APEN_A20 | 
EBI_A[19:L] pins enabled.
◆ EBI_GENERIC_APEN_A21
| #define EBI_GENERIC_APEN_A21 EBI_ROUTEPEN_APEN_A21 | 
EBI_A[20:L] pins enabled.
◆ EBI_GENERIC_APEN_A22
| #define EBI_GENERIC_APEN_A22 EBI_ROUTEPEN_APEN_A22 | 
EBI_A[21:L] pins enabled.
◆ EBI_GENERIC_APEN_A23
| #define EBI_GENERIC_APEN_A23 EBI_ROUTEPEN_APEN_A23 | 
EBI_A[22:L] pins enabled.
◆ EBI_GENERIC_APEN_A24
| #define EBI_GENERIC_APEN_A24 EBI_ROUTEPEN_APEN_A24 | 
EBI_A[23:L] pins enabled.
◆ EBI_GENERIC_APEN_A25
| #define EBI_GENERIC_APEN_A25 EBI_ROUTEPEN_APEN_A25 | 
EBI_A[24:L] pins enabled.
◆ EBI_GENERIC_APEN_A26
| #define EBI_GENERIC_APEN_A26 EBI_ROUTEPEN_APEN_A26 | 
EBI_A[25:L] pins enabled.
◆ EBI_GENERIC_APEN_A27
| #define EBI_GENERIC_APEN_A27 EBI_ROUTEPEN_APEN_A27 | 
EBI_A[26:L] pins enabled.
◆ EBI_GENERIC_APEN_A28
| #define EBI_GENERIC_APEN_A28 EBI_ROUTEPEN_APEN_A28 | 
EBI_A[27:L] pins enabled.
◆ EBI_INIT_DEFAULT
| #define EBI_INIT_DEFAULT | 
Default configuration for EBI initialization structures.
◆ EBI_TFTINIT_DEFAULT
| #define EBI_TFTINIT_DEFAULT | 
Default configuration for EBI TFT initialization structure.
Enumeration Type Documentation
◆ EBI_Mode_TypeDef
| enum EBI_Mode_TypeDef | 
◆ EBI_Polarity_TypeDef
| enum EBI_Polarity_TypeDef | 
◆ EBI_Line_TypeDef
| enum EBI_Line_TypeDef | 
EBI Pin Line types.
◆ EBI_ALow_TypeDef
| enum EBI_ALow_TypeDef | 
Address Pin Enable, lower limit - lower range of pins to enable.
◆ EBI_AHigh_TypeDef
| enum EBI_AHigh_TypeDef | 
Address Pin Enable, high limit - higher limit of pins to enable.
◆ EBI_TFTBank_TypeDef
| enum EBI_TFTBank_TypeDef | 
◆ EBI_TFTColorFormat_TypeDef
EBI TFT Color format.
◆ EBI_TFTColorSrc_TypeDef
◆ EBI_TFTInterleave_TypeDef
◆ EBI_TFTFrameBufTrigger_TypeDef
◆ EBI_TFTMaskBlend_TypeDef
Control of mask and alpha blending mode.
◆ EBI_TFTDDMode_TypeDef
◆ EBI_TFTWidth_TypeDef
| enum EBI_TFTWidth_TypeDef |