CAN_MessageObject_TypeDef Struct Reference
CAN Message Object TypeDef structure.
#include <em_can.h>
Data Fields | |
uint8_t | msgNum |
A message number of this Message Object, [1 - 32]. | |
bool | extended |
ID extended if true, standard if false. | |
uint32_t | id |
ID of the message with 11 bits (standard) or 28 bits (extended). | |
uint8_t | dlc |
Data Length Code [0 - 8]. | |
uint8_t | data [8] |
A pointer to data, [0 - 8] bytes. | |
uint32_t | mask |
A mask for ID filtering. | |
bool | extendedMask |
Enable the use of 'extended' value for filtering. | |
bool | directionMask |
Enable the use of 'direction' value for filtering. | |
CAN Message Object TypeDef structure.
LSBs is used.
Field Documentation
◆ msgNum
uint8_t CAN_MessageObject_TypeDef::msgNum |
A message number of this Message Object, [1 - 32].
◆ extended
bool CAN_MessageObject_TypeDef::extended |
ID extended if true, standard if false.
◆ id
uint32_t CAN_MessageObject_TypeDef::id |
ID of the message with 11 bits (standard) or 28 bits (extended).
LSBs are used for both.
◆ dlc
uint8_t CAN_MessageObject_TypeDef::dlc |
Data Length Code [0 - 8].
◆ data
uint8_t CAN_MessageObject_TypeDef::data[8] |
A pointer to data, [0 - 8] bytes.
◆ mask
uint32_t CAN_MessageObject_TypeDef::mask |
A mask for ID filtering.
◆ extendedMask
bool CAN_MessageObject_TypeDef::extendedMask |
Enable the use of 'extended' value for filtering.
◆ directionMask
bool CAN_MessageObject_TypeDef::directionMask |
Enable the use of 'direction' value for filtering.