EMU_VmonHystInit_TypeDef Struct Reference
VMON Hysteresis initialization structure.
      
       #include <em_emu.h>
      
     
| Data Fields | |
| EMU_VmonChannel_TypeDef | channel | 
| VMON channel to configure. | |
| int | riseThreshold | 
| Rising threshold (mV). | |
| int | fallThreshold | 
| Falling threshold (mV). | |
| bool | riseWakeup | 
| Wake up from EM4H on rising edge. | |
| bool | fallWakeup | 
| Wake up from EM4H on falling edge. | |
| bool | enable | 
| Enable VMON channel. | |
VMON Hysteresis initialization structure.
Field Documentation
◆ channel
| EMU_VmonChannel_TypeDef EMU_VmonHystInit_TypeDef::channel | 
VMON channel to configure.
◆ riseThreshold
| int EMU_VmonHystInit_TypeDef::riseThreshold | 
Rising threshold (mV).
◆ fallThreshold
| int EMU_VmonHystInit_TypeDef::fallThreshold | 
Falling threshold (mV).
◆ riseWakeup
| bool EMU_VmonHystInit_TypeDef::riseWakeup | 
Wake up from EM4H on rising edge.
◆ fallWakeup
| bool EMU_VmonHystInit_TypeDef::fallWakeup | 
Wake up from EM4H on falling edge.
◆ enable
| bool EMU_VmonHystInit_TypeDef::enable | 
Enable VMON channel.