QSPI_Init_TypeDef Struct Reference
QSPI initialization structure.
#include <em_qspi.h>
Data Fields | |
bool | enable |
Enable/disable Quad SPI when initialization is completed. | |
uint8_t | divisor |
Master mode baud rate divisor. | |
QSPI initialization structure.
Field Documentation
◆ enable
bool QSPI_Init_TypeDef::enable |
Enable/disable Quad SPI when initialization is completed.
◆ divisor
uint8_t QSPI_Init_TypeDef::divisor |
Master mode baud rate divisor.
Values can be even numbers in the range [2-32] inclusive.