ACMP_VAConfig_TypeDef Struct Reference
VA Configuration structure.
#include <em_acmp.h>
Data Fields | |
ACMP_VAInput_TypeDef | input |
VA voltage input source. | |
uint32_t | div0 |
A divider for VA voltage input source when ACMP output is 0. | |
uint32_t | div1 |
A divider for VA voltage input source when ACMP output is 1. | |
VA Configuration structure.
This structure is used to configure the VA voltage input source and its dividers.
Field Documentation
◆ input
ACMP_VAInput_TypeDef ACMP_VAConfig_TypeDef::input |
VA voltage input source.
◆ div0
uint32_t ACMP_VAConfig_TypeDef::div0 |
A divider for VA voltage input source when ACMP output is 0.
This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div0 + 1) / 64
◆ div1
uint32_t ACMP_VAConfig_TypeDef::div1 |
A divider for VA voltage input source when ACMP output is 1.
This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div1 + 1) / 64