QSPI_StigCmd_TypeDef Struct Reference
Defines command to be executed using STIG mechanism.
#include <em_qspi.h>
Data Fields | |
uint8_t | cmdOpcode |
Command op-code. | |
uint16_t | readDataSize |
Number of Read Data Bytes. | |
uint8_t | addrSize |
Number of Address Bytes. | |
uint8_t | writeDataSize |
Number of Write Data Bytes. | |
uint8_t | dummyCycles |
Number of dummy cycles. | |
bool | modeBitEnable |
Mode Bit Configuration register are sent following the address bytes. | |
uint32_t | address |
Flash command address. | |
void * | readBuffer |
Buffer for read data. | |
void * | writeBuffer |
Buffer with data to write. | |
Defines command to be executed using STIG mechanism.
Field Documentation
◆ cmdOpcode
uint8_t QSPI_StigCmd_TypeDef::cmdOpcode |
Command op-code.
◆ readDataSize
uint16_t QSPI_StigCmd_TypeDef::readDataSize |
Number of Read Data Bytes.
◆ addrSize
uint8_t QSPI_StigCmd_TypeDef::addrSize |
Number of Address Bytes.
◆ writeDataSize
uint8_t QSPI_StigCmd_TypeDef::writeDataSize |
Number of Write Data Bytes.
◆ dummyCycles
uint8_t QSPI_StigCmd_TypeDef::dummyCycles |
Number of dummy cycles.
◆ modeBitEnable
bool QSPI_StigCmd_TypeDef::modeBitEnable |
Mode Bit Configuration register are sent following the address bytes.
◆ address
uint32_t QSPI_StigCmd_TypeDef::address |
Flash command address.
◆ readBuffer
void* QSPI_StigCmd_TypeDef::readBuffer |
Buffer for read data.
◆ writeBuffer
void* QSPI_StigCmd_TypeDef::writeBuffer |
Buffer with data to write.