MSC_ExecConfig_TypeDef Struct Reference
Code execution configuration.
      
       #include <em_msc.h>
      
     
| Data Fields | |
| bool | scbtEn | 
| Enable Suppressed Conditional Branch Target Prefetch. | |
| bool | prefetchEn | 
| Enable MSC prefetching. | |
| bool | ifcDis | 
| Disable instruction cache. | |
| bool | aiDis | 
| Disable automatic cache invalidation on write or erase. | |
| bool | iccDis | 
| Disable automatic caching of fetches in interrupt context. | |
| bool | useHprot | 
| Use ahb_hprot to determine if the instruction is cacheable or not. | |
Code execution configuration.
Field Documentation
◆ scbtEn
| bool MSC_ExecConfig_TypeDef::scbtEn | 
Enable Suppressed Conditional Branch Target Prefetch.
◆ prefetchEn
| bool MSC_ExecConfig_TypeDef::prefetchEn | 
Enable MSC prefetching.
◆ ifcDis
| bool MSC_ExecConfig_TypeDef::ifcDis | 
Disable instruction cache.
◆ aiDis
| bool MSC_ExecConfig_TypeDef::aiDis | 
Disable automatic cache invalidation on write or erase.
◆ iccDis
| bool MSC_ExecConfig_TypeDef::iccDis | 
Disable automatic caching of fetches in interrupt context.
◆ useHprot
| bool MSC_ExecConfig_TypeDef::useHprot | 
Use ahb_hprot to determine if the instruction is cacheable or not.