Communication Plugin Error Codes
Description
Bootloader error codes returned by communication plugins.
Offset from BOOTLOADER_ERROR_COMMUNICATION_BASE
Macros | |
#define | BOOTLOADER_ERROR_COMMUNICATION_INIT (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x01L) |
#define | BOOTLOADER_ERROR_COMMUNICATION_START (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x02L) |
Could not start communication with host (timeout, sync error, version mismatch, ...) | |
#define | BOOTLOADER_ERROR_COMMUNICATION_DONE (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x03L) |
Host closed communication, no image received. | |
#define | BOOTLOADER_ERROR_COMMUNICATION_ERROR (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x04L) |
Unrecoverable error in host-bootloader communication. | |
#define | BOOTLOADER_ERROR_COMMUNICATION_IMAGE_ERROR (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x05L) |
Host closed communication, no valid image received. | |
#define | BOOTLOADER_ERROR_COMMUNICATION_TIMEOUT (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x06L) |
Communication aborted, no response from host. | |
Macro Definition Documentation
#define BOOTLOADER_ERROR_COMMUNICATION_INIT (BOOTLOADER_ERROR_COMMUNICATION_BASE | 0x01L) |
Invalid input parameter to security algorithm Could not initialize hardware resources for communication protocol
Definition at line 188
of file btl_errorcode.h
.