GblInputBuffer_t Struct Reference

Description

GBL parser input buffer.

Definition at line 155 of file btl_ebl_parser.h .

#include < btl_ebl_parser.h >

Data Fields

const uint8_t * buffer
Pointer to a buffer.
const size_t length
Length of the buffer.
size_t offset
Offset of the buffer.

The documentation for this struct was generated from the following file:
  • btl_ebl_parser.h