GBL Format
Description
GBL file specification.
Specification of the GBL file format. Each struct represents a valid GBL tag, and an GBL file contains a series of tags.
Data Structures | |
struct | EblTagHeader_t |
GBL tag header. Must be the first element in all GBL tags. | |
struct | EblHeader_t |
GBL header tag type. | |
struct | EblApplication_t |
GBL application tag type. | |
struct | EblBootloader_t |
GBL bootloader tag type. | |
struct | EblSeUpgrade_t |
GBL SE upgrade tag type. | |
struct | EblMetadata_t |
GBL metadata tag type. | |
struct | EblProg_t |
GBL flash program tag type. | |
struct | EblEnd_t |
GBL end tag type. | |
struct | EblEncryptionHeader_t |
GBL encryption header tag type. | |
struct | EblEncryptionInitAesCcm_t |
GBL encryption init tag type. Used with AES-CCM encryption. | |
struct | EblEncryptionData_t |
GBL encryption data tag type. | |
struct | EblEncryptionAesCcmSignature_t |
GBL encryption AES-CCM MAC tag type. | |
struct | EblCertificateEcdsaP256_t |
GBL certificate chain for signing. | |
struct | EblSignatureEcdsaP256_t |
GBL ECDSA secp256r1 signature tag type. | |
Macros | |
#define | EBL_IMAGE_MAGIC_WORD 0xE35050E3UL |
Magic word indicating GBL image. | |
#define | EBL_COMPATIBILITY_MAJOR_VERSION 0x03000000UL |
Major version of the EBL spec. | |
#define | EBLV2_COMPATIBILITY_MAJOR_VERSION 0x00000200UL |
Major version of the EBLV2 spec. | |
#define | EBL_TAG_ID_HEADER_V3 0x03A617EBUL |
Tag ID for the GBL header tag. | |
#define | EBL_TAG_ID_BOOTLOADER 0xF50909F5UL |
Tag ID for the GBL bootloader tag. | |
#define | EBL_TAG_ID_APPLICATION 0xF40A0AF4UL |
Tag ID for the GBL application info tag. | |
#define | EBL_TAG_ID_METADATA 0xF60808F6UL |
Tag ID for the GBL metadata tag. | |
#define | EBL_TAG_ID_PROG 0xFE0101FEUL |
Tag ID for the GBL flash program tag. | |
#define | EBL_TAG_ID_ERASEPROG 0xFD0303FDUL |
Tag ID for the GBL flash erase&program tag. | |
#define | EBL_TAG_ID_END 0xFC0404FCUL |
Tag ID for the GBL end tag. | |
#define | EBL_TAG_ID_SE_UPGRADE 0x5EA617EBUL |
Tag ID for the SE upgrade tag. | |
#define | EBL_TAG_ID_ENC_HEADER 0xFB0505FBUL |
Tag ID for the GBL encryption header tag. | |
#define | EBL_TAG_ID_ENC_INIT 0xFA0606FAUL |
Tag ID for the GBL encryption init tag. | |
#define | EBL_TAG_ID_ENC_EBL_DATA 0xF90707F9UL |
Tag ID for the GBL encryption data tag. | |
#define | EBL_TAG_ID_ENC_MAC 0xF70909F7UL |
Tag ID for the GBL encryption MAC tag. | |
#define | EBL_TAG_ID_SIGNATURE_ECDSA_P256 0xF70A0AF7UL |
Tag ID for the GBL ECDSA secp256r1 signature tag. | |
#define | EBL_TAG_ID_CERTIFICATE_ECDSA_P256 0xF30B0BF3UL |
Tag ID for the GBL ECDSA certfificate tag. | |
#define | EBL_TYPE_NONE 0x00000000UL |
GBL type: Standard GBL. | |
#define | EBL_TYPE_ENCRYPTION_AESCCM 0x00000001UL |
GBL type: AES-CCM encrypted GBL. | |
#define | EBL_TYPE_SIGNATURE_ECDSA 0x00000100UL |
GBL type: ECDSA P256-signed GBL. | |