Modules

The following is a list of the different bootloader APIs, both those that are internal to the bootloader, and those available to any application running alongside the bootloader.
▼ Application Interface Application interface to the bootloader
Application Parser Interface Application interface for the bootloader image parser
Application Properties Properties of the application that can be accessed by the bootloader
Application Storage Interface Application interface for interfacing with the bootloader storage
▼ Common Application Interface Generic application interface available on all versions of the bootloader, regardless of the available plugins
Reset Information Passing information when resetting into and out of the bootloader
▼ Bootloader Core Core bootloader functionality
Bootload Methods to verify and bootload application images
Flash Interface to internal flash
Reset Methods to reset from the bootloader to the app
Upgrade Methods to verify and upgrade the main bootloader
▼ Driver Hardware drivers for bootloader
Delay Basic delay functionality
SPI Basic Serial Peripheral Interface driver
SPI Slave SPI Slave Interface driver
UART Serial UART Interface driver
▼ Error Codes Bootloader error codes
Bootloading Error Codes Bootloader error codes returned by the bootloading process
Communication Plugin Error Codes Bootloader error codes returned by communication plugins
Compression Error Codes Bootloader error codes returned by the decompressor
Error Code Base Values Bootloader error code base values, per logical function
Image Parser Error Codes Bootloader error codes returned by the image file parser
Initialization Error Codes Bootloader error codes returned by initialization code
Parse Error Codes Bootloader error codes returned by image parsing
SPI Slave Driver Error Codes Bootloader error codes returned by the SPI slave driver
Security Error Codes Bootloader error codes returned by security algorithms
Storage Driver Error Codes Bootloader error codes returned by a storage driver
UART Driver Error Codes Bootloader error codes returned by the UART driver
XMODEM Error Codes Bootloader error codes returned by the XMODEM parser
▼ Plugin
▼ Communication Host communication interface
▼ Utils
▼ XMODEM Parser Parser for XMODEM packets
Commands
Debug Debug Plugin
▼ Decompressor Decompressors for Gecko Bootloader
LZ4 Decompressor LZ4 decompressor
▼ GPIO Activation Enter bootloader based on GPIO state
Button GPIO Enter bootloader based on Button GPIO state
EZSP GPIO Enter bootloader based on EZSP GPIO state
▼ Image Parser Image parser plugin
▼ GBL Parser GBL parser implementation
▼ Custom GBL Tags Handle custom GBL tags for added functionality in the GBL parser
LZ4 Programming Tag Tag to handle LZ4 compressed programming data
LZMA Programming Tag Tag to handle LZMA compressed programming data
GBL Format GBL file specification
▼ Security Collection of security plugins
AES AES decryption functionality for bootloader
CRC16 CRC16 functionality for the bootloader
CRC32 CRC32 functionality for the bootloader
Decryption Generic decryption functionality for bootloader
▼ ECDSA ECDSA signing functionality for the bootloader
ECC Library Elliptic Curve Cryptography Library
SHA_256 SHA-256 digest functionality for the bootloader
Tokens Manufacturing token handling for the bootloader
▼ Storage Storage plugin
Bootload Info Indicates which firmware update image should be bootloaded next
SPI Flash Configurations Configuration parameters for SPI flashes