Custom GBL Tags
Description
Handle custom GBL tags for added functionality in the GBL parser.
Modules | |
LZ4 Programming Tag | |
Tag to handle LZ4 compressed programming data. | |
LZMA Programming Tag | |
Tag to handle LZMA compressed programming data. | |
Data Structures | |
struct | GblCustomTag_t |
Custom tag descriptor. | |
Functions | |
bool | gbl_isCustomTag (EblTagHeader_t *tagHeader) |
const GblCustomTag_t * | gbl_getCustomTagProperties (uint32_t tagId) |
Function Documentation
bool gbl_isCustomTag | ( | EblTagHeader_t * | tagHeader | ) |
Indicate whether the GBL tag described by tagHeader is a custom tag.
- Parameters
-
tagHeader
Pointer to the GBL tag header
- Returns
- True if the tag is a custom tag, else false
const GblCustomTag_t* gbl_getCustomTagProperties | ( | uint32_t | tagId | ) |
Get properties for a custom GBL tag.
- Parameters
-
tagId
GBL Tag ID of the custom tag
- Returns
- Pointer to the custom tag descriptor