EblSeUpgrade_t Struct Reference

Description

GBL SE upgrade tag type.

Definition at line 65 of file btl_gbl_format.h .

#include < btl_gbl_format.h >

Data Fields

EblTagHeader_t header
Tag ID and length.
uint32_t blobSize
Size of the SE upgrade blob.
uint32_t version
Version of the SE image.
uint8_t * data
Array of data for SE upgrade.

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h