ApplicationProperties_t Struct Reference

Description

Application Properties struct.

Definition at line 122 of file application_properties.h .

#include < application_properties.h >

Data Fields

uint8_t magic [16]
Magic value indicating this is an ApplicationProperties_t struct. Must equal APPLICATION_PROPERTIES_MAGIC .
uint32_t structVersion
Version number of this struct.
uint32_t signatureType
Type of signature this application is signed with.
uint32_t signatureLocation
Location of the signature. Typically points to the end of the application.
ApplicationData_t app
Information about the application.
ApplicationCertificate_t * cert
Pointer to information about the certificate.
uint8_t * longTokenSectionAddress
Pointer to Long Token Data Section.

The documentation for this struct was generated from the following file:
  • application_properties.h