ApplicationCertificate Struct Reference
Description
Application Certificate.
Definition at line 108
of file application_properties.h
.
#include <
application_properties.h
>
Data Fields | |
uint8_t | structVersion |
Version of the certificate structure. | |
uint8_t | flags [3] |
Reserved flags. | |
uint8_t | key [64] |
Public key. | |
uint32_t | version |
The version number of this certificate. | |
uint8_t | signature [64] |
Signature of the certificate. | |
The documentation for this struct was generated from the following file:
application_properties.h