Description

Manufacturing token handling for the bootloader.

Functions

const uint8_t * btl_getSignedBootloaderKeyXPtr (void)
const uint8_t * btl_getSignedBootloaderKeyYPtr (void)
const uint8_t * btl_getImageFileEncryptionKeyPtr (void)

Function Documentation

const uint8_t* btl_getSignedBootloaderKeyXPtr ( void )

Get the X component of the ECDSA secp256r1 public key.

Returns
Pointer to X component of the public key
const uint8_t* btl_getSignedBootloaderKeyYPtr ( void )

Get the Y component of the ECDSA secp256r1 public key.

Returns
Pointer to Y component of the public key
const uint8_t* btl_getImageFileEncryptionKeyPtr ( void )

Get the AES-CCM encryption key.

Returns
Pointer to the AES-CCM key