EblBootloader_t Struct Reference
Description
GBL bootloader tag type.
Definition at line 57
of file btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields | |
EblTagHeader_t | header |
Tag ID and length. | |
uint32_t | bootloaderVersion |
Version number of the bootloader. | |
uint32_t | address |
Address of the bootloader. | |
uint8_t * | data |
Array of data for bootloader upgrade. | |
The documentation for this struct was generated from the following file:
btl_gbl_format.h