XMODEM Error Codes
Description
Bootloader error codes returned by the XMODEM parser.
Offset from BOOTLOADER_ERROR_XMODEM_BASE
Macros | |
#define | BOOTLOADER_ERROR_XMODEM_CRCL (BOOTLOADER_ERROR_XMODEM_BASE | 0x01L) |
Could not verify lower CRC byte. | |
#define | BOOTLOADER_ERROR_XMODEM_CRCH (BOOTLOADER_ERROR_XMODEM_BASE | 0x02L) |
Could not verify upper CRC byte. | |
#define | BOOTLOADER_ERROR_XMODEM_NO_SOH (BOOTLOADER_ERROR_XMODEM_BASE | 0x03L) |
No start of header found. | |
#define | BOOTLOADER_ERROR_XMODEM_PKTNUM (BOOTLOADER_ERROR_XMODEM_BASE | 0x04L) |
Packet number doesn't match its inverse. | |
#define | BOOTLOADER_ERROR_XMODEM_PKTSEQ (BOOTLOADER_ERROR_XMODEM_BASE | 0x05L) |
Packet number error (unexpected sequence) | |
#define | BOOTLOADER_ERROR_XMODEM_PKTDUP (BOOTLOADER_ERROR_XMODEM_BASE | 0x06L) |
Packet number error (duplicate) | |
#define | BOOTLOADER_ERROR_XMODEM_DONE (BOOTLOADER_ERROR_XMODEM_BASE | 0x07L) |
Transfer is done (Technically not an error) | |
#define | BOOTLOADER_ERROR_XMODEM_CANCEL (BOOTLOADER_ERROR_XMODEM_BASE | 0x08L) |
Transfer is canceled. | |