ImageProperties_t Struct Reference
Description
Structure containing state of the image file processed.
Definition at line 41
of file btl_image_parser.h
.
#include <
btl_image_parser.h
>
Data Fields | |
uint8_t | contents |
Image contents. | |
uint8_t | instructions |
Parser instructions. | |
bool | imageCompleted |
Flag to indicate parsing has completed. | |
bool | imageVerified |
Flag to indicate the image file has been validated. | |
uint32_t | bootloaderVersion |
Version number of main bootloader extracted from image file. | |
ApplicationData_t | application |
Information about the application. | |
uint32_t | bootloaderUpgradeSize |
Size of the bootloader upgrade contained in the image file. | |
uint32_t | seUpgradeVersion |
Version number of SE upgrade extracted from image file. | |
The documentation for this struct was generated from the following file:
btl_image_parser.h