EblEncryptionInitAesCcm_t Struct Reference
Description
GBL encryption init tag type. Used with AES-CCM encryption.
Definition at line 100
of file btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields | |
EblTagHeader_t | header |
Tag ID and length. | |
uint32_t | msgLen |
Length of the cipher text in bytes. | |
uint8_t | nonce [12] |
Random nonce used for AES-CTR in this message. | |
The documentation for this struct was generated from the following file:
btl_gbl_format.h