UART Driver Error Codes

Description

Bootloader error codes returned by the UART driver.

Offset from BOOTLOADER_ERROR_UART_BASE

Macros

#define BOOTLOADER_ERROR_UART_UNINIT ( BOOTLOADER_ERROR_UART_BASE | 0x01)
Operation not allowed because hardware has not been initialized.
#define BOOTLOADER_ERROR_UART_INIT ( BOOTLOADER_ERROR_UART_BASE | 0x02)
Hardware fail during initialization.
#define BOOTLOADER_ERROR_UART_ARGUMENT ( BOOTLOADER_ERROR_UART_BASE | 0x03)
Invalid argument.
#define BOOTLOADER_ERROR_UART_TIMEOUT ( BOOTLOADER_ERROR_UART_BASE | 0x04)
Operation timed out.
#define BOOTLOADER_ERROR_UART_OVERFLOW ( BOOTLOADER_ERROR_UART_BASE | 0x05)
Buffer overflow condition.
#define BOOTLOADER_ERROR_UART_BUSY ( BOOTLOADER_ERROR_UART_BASE | 0x06)
Busy condition.