ApplicationData Struct Reference

Description

Application Data.

Definition at line 95 of file application_properties.h .

#include < application_properties.h >

Data Fields

uint32_t type
Bitfield representing type of application, e.g., APPLICATION_TYPE_ZIGBEE .
uint32_t version
Version number for this application.
uint32_t capabilities
Capabilities of this application.
uint8_t productId [16]
Unique ID (UUID or GUID) for the product this application is built for.

The documentation for this struct was generated from the following file:
  • application_properties.h