BootloadBootloader Core
Description
Methods to verify and bootload application images.
Functions |
|
bool | bootload_verifyApplication (uint32_t startAddress) |
void | bootload_bootloaderCallback (uint32_t offset, uint8_t data[], size_t length, void *context) |
void | bootload_applicationCallback (uint32_t address, uint8_t data[], size_t length, void *context) |
bool | bootloader_enforceSecureBoot (void) |
bool | bootload_commitBootloaderUpgrade (uint32_t upgradeAddress, uint32_t size) |
bool | bootload_checkSeUpgradeVersion (uint32_t upgradeVersion) |
bool | bootload_commitSeUpgrade (uint32_t upgradeAddress) |
Function Documentation
bool bootload_verifyApplication | ( | uint32_t |
startAddress
|
) |
Verify the application image stored in the flash memory starting at the address startAddress.
If secure boot is enforced, the function will only return true if the cryptographic signature of the application is valid. Else, the application is verified according to the signature type defined in the ApplicationProperties_t structure embedded in the application. Silicon Labs wireless stacks take care of declaring this structure. Applications not using a full wireless stack may need to instantiate the structure themselves.
Examples of results when secure boot is not enforced:
- App has no signature: Valid if initial stack pointer and program counter have reasonable values
- App has CRC checksum: Valid if checksum is valid
- App has ECDSA signature: Valid if ECDSA signature is valid.
When secure boot is enforced, only ECDSA signed applications with a valid signature are considered valid.
- Parameters
-
[in] startAddress
Starting address of the application
- Returns
- True if the image is deemed valid
void bootload_bootloaderCallback | ( | uint32_t |
offset,
|
uint8_t |
data[],
|
||
size_t |
length,
|
||
void * |
context
|
||
) |
Bootloader upgrade callback implementation
- Parameters
-
offset
Offset of bootloader data (byte counter incrementing from 0) data
Raw bootloader data length
Size in bytes of raw bootloader data. context
A context variable defined by the implementation that is implementing this callback.
void bootload_applicationCallback | ( | uint32_t |
address,
|
uint8_t |
data[],
|
||
size_t |
length,
|
||
void * |
context
|
||
) |
Image data callback implementation
- Parameters
-
address
Address (inside the raw image) the data starts at data
Raw image data length
Size in bytes of raw image data. Constrained to always be a multiple of four. context
A context variable defined by the implementation that is implementing this callback.
bool bootloader_enforceSecureBoot | ( | void |
|
) |
Whether the bootloader should enforce secure boot
- Returns
- True if secure boot is to be enforced
bool bootload_commitBootloaderUpgrade | ( | uint32_t |
upgradeAddress,
|
uint32_t |
size
|
||
) |
Perform a bootloader upgrade using the upgrade image present at upgradeAddress with length size.
If the bootloader upgrade process starts successfully, this function does not return, and execution will resume from the reset handler of the upgraded bootloader.
- Parameters
-
[in] upgradeAddress
The starting address of the upgrade image [in] size
The length of the upgrade image in bytes
- Returns
- False if the bootloader upgrade process didn't start
bool bootload_checkSeUpgradeVersion | ( | uint32_t |
upgradeVersion
|
) |
Check that an SE upgrade with a given version number is allowed to be installed.
This will only be true if the upgrade version is higher than the running version.
- Parameters
-
[in] upgradeVersion
The version of the SE upgrade image
- Returns
- True if the SE upgrade image should be installed
bool bootload_commitSeUpgrade | ( | uint32_t |
upgradeAddress
|
) |
Perform an SE upgrade using the upgrade image present at upgradeAddress.
If the SE upgrade process starts successfully, this function does not return, and execution will resume from the reset handler after the SE upgrade is complete.
- Parameters
-
[in] upgradeAddress
The starting address of the upgrade image
- Returns
- False if the SE upgrade process didn't start