SPI SlaveDriver
Description
SPI Slave Interface driver.
Flexible SPI Slave driver implementation for use in an NCP scenario.
This driver will support both blocking and non-blocking operation, with LDMA backing the background transfers to support nonblocking.
Functions |
|
| void | spislave_init (void) |
| void | spislave_deinit (void) |
| int32_t | spislave_sendBuffer (uint8_t *buffer, size_t length) |
| int32_t | spislave_sendByte (uint8_t byte) |
| size_t | spislave_getTxBytesLeft (void) |
| void | spislave_enableTransmitter (bool enable) |
| void | spislave_enableReceiver (bool enable) |
| size_t | spislave_getRxAvailableBytes (void) |
| int32_t | spislave_receiveBuffer (uint8_t *buffer, size_t requestedLength, size_t *receivedLength, bool blocking, uint32_t timeout) |
| int32_t | spislave_receiveByte (uint8_t *byte) |
| void | spislave_flush (bool flushTx, bool flushRx) |
Function Documentation
| void spislave_init | ( | void |
|
) |
Initialize the configured USART peripheral for SPI slave operation. Also sets up GPIO settings for MOSI, MISO, SCLK and SS. After initialization, the SPI slave will have RX enabled.
- Returns
- BOOTLOADER_OK if succesful, error code otherwise
| void spislave_deinit | ( | void |
|
) |
Disable the configured USART peripheral for SPI operation.
| int32_t spislave_sendBuffer | ( | uint8_t * |
buffer,
|
| size_t |
length
|
||
| ) |
Write a data buffer to the master next time the master starts clocking SCLK. This transfer will be non-blocking, and its progress can be tracked through spislave_getTxBytesLeft
- Parameters
-
[in] bufferThe data buffer to send [in] lengthNumber of bytes in the buffer to send
- Returns
- BOOTLOADER_OK if successful, error code otherwise
| int32_t spislave_sendByte | ( | uint8_t |
byte
|
) |
Write one byte to the master in a blocking fashion.
- Warning
- If the master goes down, this will block forever.
- Parameters
-
[in] byteThe byte to send
- Returns
- BOOTLOADER_OK if succesful, error code otherwise
| size_t spislave_getTxBytesLeft | ( | void |
|
) |
Gets the amount of bytes left in the TX data buffer.
- Returns
- Number of bytes in the transmit buffer still needing to go out
| void spislave_enableTransmitter | ( | bool |
enable
|
) |
Enable/disable MISO output
- Parameters
-
[in] enableTrue to enable the transmitter, false to disable
| void spislave_enableReceiver | ( | bool |
enable
|
) |
Enable/disable receiving bytes from the master into our internal buffer. The purpose of this function is to avoid filling up the buffer with 0xFF while a master is polling for new data.
- Parameters
-
[in] enableTrue to enable the receiver, false to disable
| size_t spislave_getRxAvailableBytes | ( | void |
|
) |
Gets the amount of bytes ready for reading.
- Returns
- Number of bytes in the receive buffer available for reading with spislave_receiveBuffer
| int32_t spislave_receiveBuffer | ( | uint8_t * |
buffer,
|
| size_t |
requestedLength,
|
||
| size_t * |
receivedLength,
|
||
| bool |
blocking,
|
||
| uint32_t |
timeout
|
||
| ) |
Read from the RX buffer into a local buffer.
- Parameters
-
[out] bufferThe data buffer to receive into [in] requestedLengthNumber of bytes we'd like to read [out] receivedLengthNumber of bytes read [in] blockingIndicate whether we should wait for requestedLength bytes to be available and read before returning, or we can read out whatever is currently in the buffer and return. [in] timeoutNumber of milliseconds to wait for data in blocking mode
- Returns
- BOOTLOADER_OK if succesful, error code otherwise
| int32_t spislave_receiveByte | ( | uint8_t * |
byte
|
) |
Get one byte from the SPI slave in a blocking fashion.
- Warning
- If the master never clocks in a byte, this function will block forever.
- Parameters
-
[out] bytePointer to where to put the received byte
- Returns
- BOOTLOADER_OK if succesful, error code otherwise
| void spislave_flush | ( | bool |
flushTx,
|
| bool |
flushRx
|
||
| ) |
Flush one or both buffers.
- Parameters
-
[in] flushTxFlush the transmit buffer when true [in] flushRxFlush the receive buffer when true