Application Storage InterfaceApplication Interface
Description
Application interface for interfacing with the bootloader storage.
The Storage Interface is only available on bootloaders that declare they support BOOTLOADER_CAPABILITY_STORAGE .
Data Structures |
|
| struct | BootloaderStorageSlot_t |
|
Information about a storage slot.
|
|
| struct | BootloaderStorageImplementationInformation_t |
|
Information about the bootloader storage implementation.
|
|
| struct | BootloaderStorageInformation_t |
|
Information about the bootloader storage.
|
|
| struct | BootloaderEraseStatus_t |
|
Erase status struct.
|
|
| struct | BootloaderStorageFunctions |
|
Storage API accessible from the application.
|
|
Macros |
|
| #define | BOOTLOADER_STORAGE_IMPL_INFO_VERSION (0x0201) |
|
Current version of the
BootloaderStorageImplementationInformation_t
struct.
|
|
| #define | BOOTLOADER_STORAGE_IMPL_INFO_VERSION_MAJOR (0x0200) |
|
Major version of the
BootloaderStorageImplementationInformation_t
struct.
|
|
| #define | BOOTLOADER_STORAGE_IMPL_INFO_VERSION_MAJOR_MASK (0xFF00) |
|
Major version mask for
BOOTLOADER_STORAGE_IMPL_INFO_VERSION
.
|
|
| #define | BOOTLOADER_STORAGE_IMPL_CAPABILITY_ERASE_SUPPORTED (1 << 0) |
|
Spiflash capability indicating that it supports erase.
|
|
| #define | BOOTLOADER_STORAGE_IMPL_CAPABILITY_PAGE_ERASE_REQUIRED (1 << 1) |
|
Spiflash capability indicating it requires full page erases before new data can be written.
|
|
| #define | BOOTLOADER_STORAGE_IMPL_CAPABILITY_BLOCKING_WRITE (1 << 2) |
|
Spiflash capability indicating that the write function is blocking.
|
|
| #define | BOOTLOADER_STORAGE_IMPL_CAPABILITY_BLOCKING_ERASE (1 << 3) |
|
Spiflash capability indicating that the erase function is blocking.
|
|
| #define | BOOTLOADER_STORAGE_VERIFICATION_CONTEXT_SIZE (384) |
|
Context size for bootloader verification context.
|
|
Typedefs |
|
| typedef struct BootloaderStorageFunctions | BootloaderStorageFunctions_t |
|
Storage API accessible from the application.
|
|
Enumerations |
|
| enum |
BootloaderStorageType_t
{
SPIFLASH , INTERNAL_FLASH , CUSTOM_STORAGE } |
|
Possible storage types.
|
|
Functions |
|
| void | bootloader_getStorageInfo ( BootloaderStorageInformation_t *info) |
| int32_t | bootloader_getStorageSlotInfo (uint32_t slotId, BootloaderStorageSlot_t *slot) |
| int32_t | bootloader_readStorage (uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length) |
| int32_t | bootloader_writeStorage (uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length) |
| int32_t | bootloader_eraseWriteStorage (uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length) |
| int32_t | bootloader_eraseStorageSlot (uint32_t slotId) |
| int32_t | bootloader_initChunkedEraseStorageSlot (uint32_t slotId, BootloaderEraseStatus_t *eraseStat) |
| int32_t | bootloader_chunkedEraseStorageSlot ( BootloaderEraseStatus_t *eraseStat) |
| int32_t | bootloader_setImagesToBootload (int32_t *slotIds, size_t length) |
| int32_t | bootloader_getImagesToBootload (int32_t *slotIds, size_t length) |
| int32_t | bootloader_appendImageToBootloadList (int32_t slotId) |
| int32_t | bootloader_setImageToBootload (int32_t slotId) |
| int32_t | bootloader_initVerifyImage (uint32_t slotId, void *context, size_t contextSize) |
| int32_t | bootloader_continueVerifyImage (void *context, BootloaderParserCallback_t metadataCallback) |
| int32_t | bootloader_verifyImage (uint32_t slotId, BootloaderParserCallback_t metadataCallback) |
| int32_t | bootloader_getImageInfo (uint32_t slotId, ApplicationData_t *appInfo, uint32_t *bootloaderVersion) |
| bool | bootloader_storageIsBusy (void) |
| int32_t | bootloader_readRawStorage (uint32_t address, uint8_t *buffer, size_t length) |
| int32_t | bootloader_writeRawStorage (uint32_t address, uint8_t *buffer, size_t length) |
| int32_t | bootloader_eraseRawStorage (uint32_t address, size_t length) |
Enumeration Type Documentation
Function Documentation
| void bootloader_getStorageInfo | ( | BootloaderStorageInformation_t * |
info
|
) |
Get information about the storage plugin.
- Parameters
-
[out] infoInformation about the storage plugin.
| int32_t bootloader_getStorageSlotInfo | ( | uint32_t |
slotId,
|
| BootloaderStorageSlot_t * |
slot
|
||
| ) |
Get information about a storage slot.
- Parameters
-
[in] slotIdID of the slot to get information about [out] slotInformation about the storage slot.
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_readStorage | ( | uint32_t |
slotId,
|
| uint32_t |
offset,
|
||
| uint8_t * |
buffer,
|
||
| size_t |
length
|
||
| ) |
Read data from a storage slot.
- Parameters
-
[in] slotIdID of the slot [in] offsetOffset into the slot to start reading from [out] bufferBuffer to store the data [in] lengthHow much data to read
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_writeStorage | ( | uint32_t |
slotId,
|
| uint32_t |
offset,
|
||
| uint8_t * |
buffer,
|
||
| size_t |
length
|
||
| ) |
Write data to a storage slot.
- Parameters
-
[in] slotIdID of the slot [in] offsetOffset into the slot to start writing to [in] bufferBuffer to read data to write from [in] lengthHow much data to write
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_eraseWriteStorage | ( | uint32_t |
slotId,
|
| uint32_t |
offset,
|
||
| uint8_t * |
buffer,
|
||
| size_t |
length
|
||
| ) |
Erase and write data to a storage slot.
- Note
- This function automatically erases the following flash page whenever the written data crosses a page boundary. This means that the function cannot be used to perform multiple sequential writes to the same address range unless the range starts at a page boundary. For a sequential write, the first call to this function should have a start address at a page boundary, otherwise the corresponding page of the starting address needs to be erased explicitly.
- Parameters
-
[in] slotIdID of the slot [in] offsetOffset into the slot to start writing to [in] bufferBuffer to read data to write from [in] lengthHow much data to write
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_eraseStorageSlot | ( | uint32_t |
slotId
|
) |
Erase all contents of a storage slot.
- Parameters
-
[in] slotIdID of the slot
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_initChunkedEraseStorageSlot | ( | uint32_t |
slotId,
|
| BootloaderEraseStatus_t * |
eraseStat
|
||
| ) |
Initialize chunked erase of a storage slot.
- Note
- This function must be called before calling bootloader_chunkedEraseStorageSlot in a loop.
- Parameters
-
[in] slotIdID of the slot [in] eraseStatErase status struct
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_chunkedEraseStorageSlot | ( | BootloaderEraseStatus_t * |
eraseStat
|
) |
Erase one page from a storage slot according to the struct BootloaderEraseStatus_t .
- Note
- bootloader_initChunkedEraseStorageSlot must be called before calling this function, in order to prepare BootloaderEraseStatus_t .
- This can be called sequentially to e.g. erase all the contents of a storage slot.
- Parameters
-
[in] eraseStatErase status struct
- Returns
- BOOTLOADER_ERROR_STORAGE_CONTINUE if erasing a page was successful. Erase can be continued by calling this function again. BOOTLOADER_OK if the entire slot has been erased, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_setImagesToBootload | ( | int32_t * |
slotIds,
|
| size_t |
length
|
||
| ) |
Set a prioritized list of images to attempt to bootload. The last call to this function determines which slot will be installed when bootloader_rebootAndInstall is called.
- Parameters
-
[in] slotIdsPrioritized list of slot IDs to attempt to bootload. The first image to pass verification will be bootloaded. [in] lengthLength of the slotIds array
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_BOOTLOAD_BASE range
| int32_t bootloader_getImagesToBootload | ( | int32_t * |
slotIds,
|
| size_t |
length
|
||
| ) |
Get the prioritized list of images the bootloader will attempt to bootload.
- Parameters
-
[out] slotIdsPrioritized list of slot IDs to attempt to bootload. The first image to pass verification will be bootloaded. [in] lengthLength of the slotIds array
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_BOOTLOAD_BASE range
| int32_t bootloader_appendImageToBootloadList | ( | int32_t |
slotId
|
) |
Append a single image to the list of images to attempt to bootload.
- Parameters
-
[in] slotIdID of the slot to append
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_BOOTLOAD_BASE range
| int32_t bootloader_setImageToBootload | ( | int32_t |
slotId
|
) |
Set a single image to attempt to bootload.
- Parameters
-
[in] slotIdID of the slot
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_BOOTLOAD_BASE range
| int32_t bootloader_initVerifyImage | ( | uint32_t |
slotId,
|
| void * |
context,
|
||
| size_t |
contextSize
|
||
| ) |
Initialize image verification.
Initialize verification of an upgrade image stored in a bootloader storage slot.
- Note
- This function must be called before calling bootloader_continueVerifyImage in a loop.
- The context pointer must point to memory allocated by the caller. The required size of this context may depend on the version of the bootloader. The required size for the bootloader associated with this version of the application interface is given by the define BOOTLOADER_STORAGE_VERIFICATION_CONTEXT_SIZE .
- Instead of calling bootloader_initVerifyImage followed by bootloader_continueVerifyImage , a single call to bootloader_verifyImage can be performed if the caller doesn't have any time-critical tasks to attend to, and has sufficient stack space for the automatically allocated context. The purpose of the init-and-continue functions is to allow the caller to service system needs during verification.
- Parameters
-
[in] slotIdId of the slot to check. contextPointer to memory used to hold the parser context. [in] contextSizeSize of the context. An error is returned if the supplied context is too small.
- Returns
- BOOTLOADER_OK if the image parser was initialized, else error code.
| int32_t bootloader_continueVerifyImage | ( | void * |
context,
|
| BootloaderParserCallback_t |
metadataCallback
|
||
| ) |
Continue image verification.
Continue verification of an upgrade image stored in a bootloader storage slot.
- Note
- This function must be called in a loop until anything other than BOOTLOADER_ERROR_PARSE_CONTINUE is returned.
- bootloader_initVerifyImage must be called before calling this function, in order to reset the parser.
- Instead of calling bootloader_initVerifyImage followed by bootloader_continueVerifyImage , a single call to bootloader_verifyImage can be performed if the caller doesn't have any time-critical tasks to attend to. The purpose of the init-and-continue functions is to allow the caller to service system needs during verification.
- Parameters
-
contextPointer to context structure that has previously been initialized by calling bootloader_initVerifyImage() [in] metadataCallbackFunction pointer which gets called when there is binary metadata present in the image being verified. Set to NULL if not required.
- Returns
- BOOTLOADER_ERROR_PARSE_CONTINUE if parsing was successful, and the parser expects more data. BOOTLOADER_ERROR_PARSE_SUCCESS if the parser has successfully parsed the image and it passes verification. Else error code.
| int32_t bootloader_verifyImage | ( | uint32_t |
slotId,
|
| BootloaderParserCallback_t |
metadataCallback
|
||
| ) |
Verify that the image in the given storage slot is valid
- Parameters
-
[in] slotIdId of the slot to check [in] metadataCallbackFunction pointer which gets called when there is binary metadata present in the storage slot. Set to NULL if not required.
- Note
- This function will allocate a context structure of the size given by BOOTLOADER_STORAGE_VERIFICATION_CONTEXT_SIZE on the caller's stack. If the caller prefers to manage its own memory, and allocate the context elsewhere (on the heap, as a global variable, etc), use the bootloader_initVerifyImage and bootloader_continueVerifyImage functions instead.
- Returns
- BOOTLOADER_OK if the image is valid, else error code.
| int32_t bootloader_getImageInfo | ( | uint32_t |
slotId,
|
| ApplicationData_t * |
appInfo,
|
||
| uint32_t * |
bootloaderVersion
|
||
| ) |
Get application and bootloader upgrade metadata from storage slot
- Parameters
-
[in] slotIdId of the slot to check [out] appInfoPointer to ApplicationData_t struct [out] bootloaderVersionPointer to integer representing bootloader version
- Returns
- BOOTLOADER_OK if metadata was filled successfully
| bool bootloader_storageIsBusy | ( | void |
|
) |
Check whether the bootloader storage is busy
- Returns
- True if the storage is busy
| int32_t bootloader_readRawStorage | ( | uint32_t |
address,
|
| uint8_t * |
buffer,
|
||
| size_t |
length
|
||
| ) |
Read raw data from storage.
- Parameters
-
[in] addressAddress to start reading from [out] bufferBuffer to store the data [in] lengthHow much data to read
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_writeRawStorage | ( | uint32_t |
address,
|
| uint8_t * |
buffer,
|
||
| size_t |
length
|
||
| ) |
Write data to storage.
- Parameters
-
[in] addressAddress to start writing to [in] bufferBuffer to read data to write from [in] lengthHow much data to write
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t bootloader_eraseRawStorage | ( | uint32_t |
address,
|
| size_t |
length
|
||
| ) |
Erase data from storage.
- Note
- Erasing storage must adhere to the limitiations of the underlying storage medium, such as requiring full page erases. Use bootloader_getStorageInfo to learn the limitiations of the configured storage medium.
- Parameters
-
[in] addressAddress to start erasing from [in] lengthLength of data to erase
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range