BootloaderEraseStatus_t Struct ReferenceApplication Interface > Application Storage Interface
Description
Erase status struct.
Definition at line 91
of file btl_interface_storage.h
.
#include <
btl_interface_storage.h
>
Data Fields | |
uint32_t | currentPageAddr |
Address of the current page to be erased. | |
uint32_t | pageSize |
The size of a single erasable page in bytes. | |
BootloaderStorageSlot_t | storageSlotInfo |
Information about a storage slot. | |
The documentation for this struct was generated from the following file:
btl_interface_storage.h