BootloadInfo_t Struct ReferencePlugin > Storage > Bootload Info

Description

Definition of the Bootload Info struct.

The Bootload Info struct contains a prioritized list of firmware update images that the bootloader should attempt to bootload. The first image to pass verification will be bootloaded.

Definition at line 65 of file btl_storage_bootloadinfo.h .

#include < btl_storage_bootloadinfo.h >

Data Fields

uint32_t magic
Magic word indicating that this is a Bootload Info struct ( BTL_STORAGE_BOOTLOADINFO_MAGIC )
uint32_t structVersion
Struct version number.
uint32_t length
Size of the BootloadInfo_t struct.
int32_t bootloadList [ BTL_STORAGE_BOOTLOAD_LIST_MAX_LENGTH ]
List of addresses of slots to bootload from.
uint32_t crc32
Checksum of the struct.

The documentation for this struct was generated from the following file:
  • btl_storage_bootloadinfo.h