CommunicationPlugin
Description
Host communication interface.
The Communication plugin provides an interface for implementing communication with a host device, such as a computer or a microcontroller.
Communication Protocol Implementations
Several plugins implement the communication interface, using different transports and protocols.
BGAPI UART DFU
By enabling the BGAPI communication plugin, the bootloader communication interface implements the UART DFU protocol using BGAPI commands. This plugin makes the bootloader compatible with the legacy UART bootloader that was previously released with the Silicon Labs Bluetooth stack.
EZSP-SPI
By enabling the EZSP-SPI communication plugin, the bootloader communication interface implements the EZSP protocol over SPI. This plugin makes the bootloader compatible with the legacy
ezsp-spi-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks. UART XMODEM
By enabling the UART XMODEM communication plugin, the bootloader communication interface implements the XMODEM-CRC protocol over UART. This plugin makes the bootloader compatible with the legacy
serial-uart-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks. Modules | |
Utils | |
Functions | |
void | communication_init (void) |
int32_t | communication_start (void) |
int32_t | communication_main (void) |
void | communication_shutdown (void) |
Function Documentation
void communication_init | ( | void |
| ) |
Initialize hardware for the communication plugin.
int32_t communication_start | ( | void |
| ) |
Initialize communication between the bootloader and external host. E.g. indicate to the external host that we're alive and kicking.
- Returns
- Error code indicating success or failure
- Return values
-
BOOTLOADER_OK
on success BOOTLOADER_ERROR_COMMUNICATION_START
on failure
int32_t communication_main | ( | void |
| ) |
This function is not supposed to return until the host signals the end of the current session, or a new image has been flashed and verified.
- Returns
- Error code indicating sucess or failure
- Return values
-
BOOTLOADER_OK
when a new image was flashed BOOTLOADER_ERROR_COMMUNICATION_ERROR
on communication error BOOTLOADER_ERROR_COMMUNICATION_DONE
when no image was received BOOTLOADER_ERROR_COMMUNICATION_IMAGE_ERROR
when received image is invalid
void communication_shutdown | ( | void |
| ) |
Stop communication between the bootloader and external host.