EblEncryptionInitAesCcm_t Struct ReferencePlugin > Image Parser > GBL Parser > GBL Format

Description

GBL encryption init tag type. Used with AES-CCM encryption.

Definition at line 100 of file btl_gbl_format.h .

#include < btl_gbl_format.h >

Data Fields

EblTagHeader_t header
Tag ID and length.
uint32_t msgLen
Length of the cipher text in bytes.
uint8_t nonce [12]
Random nonce used for AES-CTR in this message.

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h