EblProg_t Struct ReferencePlugin > Image Parser > GBL Parser > GBL Format
Description
GBL flash program tag type.
Definition at line 79
of file btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields | |
EblTagHeader_t | header |
Tag ID and length. | |
uint32_t | flashStartAddress |
Address to start flashing. | |
uint8_t * | data |
Array of data to flash. | |
The documentation for this struct was generated from the following file:
btl_gbl_format.h