ImageProperties_t Struct ReferencePlugin > Image Parser

Description

Structure containing state of the image file processed.

Definition at line 41 of file btl_image_parser.h .

#include < btl_image_parser.h >

Data Fields

uint8_t contents
Image contents.
uint8_t instructions
Parser instructions.
bool imageCompleted
Flag to indicate parsing has completed.
bool imageVerified
Flag to indicate the image file has been validated.
uint32_t bootloaderVersion
Version number of main bootloader extracted from image file.
ApplicationData_t application
Information about the application.
uint32_t bootloaderUpgradeSize
Size of the bootloader upgrade contained in the image file.
uint32_t seUpgradeVersion
Version number of SE upgrade extracted from image file.

The documentation for this struct was generated from the following file:
  • btl_image_parser.h