DelayDriver
Description
Basic delay functionality.
Simple delay routines for use with plugins that require small delays.
Functions |
|
| void | delay_microseconds (uint32_t usecs) |
| void | delay_init (void) |
| void | delay_milliseconds (uint32_t msecs, bool blocking) |
| bool | delay_expired (void) |
Function Documentation
| void delay_microseconds | ( | uint32_t |
usecs
|
) |
Delay for a number of microseconds
- Note
- This function can be used without calling delay_init() first.
- Parameters
-
usecsNumber of microseconds to delay
| void delay_init | ( | void |
|
) |
Initialize the delay driver's millisecond counter
| void delay_milliseconds | ( | uint32_t |
msecs,
|
| bool |
blocking
|
||
| ) |
Delay for a number of milliseconds
- Parameters
-
msecsNumber of milliseconds to delay blockingWhether to block until the delay has expired. If false, the delay_expired() function can be called to check whether the delay has expired.
| bool delay_expired | ( | void |
|
) |
Check whether the current delay has expired
- Returns
- True if the delay has expired