SPIDriver
Description
Basic Serial Peripheral Interface driver.
Simple, blocking SPI master implementation for communication with external devices.
Functions |
|
| void | spi_init (void) |
| void | spi_deinit (void) |
| void | spi_writeByte (uint8_t data) |
| void | spi_writeHalfword (uint16_t data) |
| void | spi_write3Byte (uint32_t data) |
| uint8_t | spi_readByte (void) |
| uint16_t | spi_readHalfword (void) |
| void | spi_setCsActive (void) |
| void | spi_setCsInactive (void) |
Function Documentation
| void spi_init | ( | void |
|
) |
Initialize a USART peripheral for SPI
| void spi_deinit | ( | void |
|
) |
De-initialize a USART peripheral for SPI
| void spi_writeByte | ( | uint8_t |
data
|
) |
Write a single byte, discarding the received byte
- Parameters
-
[in] dataThe byte to send
| void spi_writeHalfword | ( | uint16_t |
data
|
) |
Write two bytes, discarding the received bytes
- Parameters
-
[in] dataThe bytes to send, most significant byte first
| void spi_write3Byte | ( | uint32_t |
data
|
) |
Write three bytes, discarding the received bytes
- Parameters
-
[in] dataThe bytes to send, most significant byte first
| uint8_t spi_readByte | ( | void |
|
) |
Read a byte by sending a 0xFF byte
- Returns
- The received byte
| uint16_t spi_readHalfword | ( | void |
|
) |
Read two bytes by sending two 0xFF bytes
- Returns
- The received bytes, most significant byte first
| void spi_setCsActive | ( | void |
|
) |
Assert the slave select line. Polarity is configured by spi_init .
| void spi_setCsInactive | ( | void |
|
) |
Dessert the slave select line. Polarity is configured by spi_init .