Image ParserPlugin
Description
Image parser plugin.
Generic image parser interface for Silicon Labs bootloader.
Modules |
|
| GBL Parser | |
|
GBL parser implementation.
|
|
Data Structures |
|
| struct | ImageProperties_t |
|
Structure containing state of the image file processed.
|
|
Macros |
|
| #define | BTL_IMAGE_CONTENT_APPLICATION 0x01U |
|
Upgrade image contains application upgrade.
|
|
| #define | BTL_IMAGE_CONTENT_BOOTLOADER 0x02U |
|
Upgrade image contains bootloader upgrade.
|
|
| #define | BTL_IMAGE_CONTENT_SE 0x04U |
|
Upgrade image contains SE upgrade.
|
|
| #define | BTL_IMAGE_INSTRUCTION_APPLICATION 0x01U |
|
Application upgrade should be applied from upgrade image.
|
|
| #define | BTL_IMAGE_INSTRUCTION_BOOTLOADER 0x02U |
|
Bootloader upgrade should be applied from upgrade image.
|
|
| #define | BTL_IMAGE_INSTRUCTION_SE 0x04U |
|
SE upgrade should be applied from upgrade image.
|
|
Functions |
|
| int32_t | parser_init (void *context, void *decryptContext, void *authContext, uint8_t flags) |
| int32_t | parser_parse (void *context, ImageProperties_t *imageProperties, uint8_t buffer[], size_t length, const BootloaderParserCallbacks_t *callbacks) |
| bool | parser_requireAuthenticity (void) |
| bool | parser_requireConfidentiality (void) |
| uint32_t | parser_getApplicationAddress (void) |
| uint32_t | parser_getBootloaderUpgradeAddress (void) |
| bool | parser_applicationUpgradeValidCallback ( ApplicationData_t *app) |
Function Documentation
| int32_t parser_init | ( | void * |
context,
|
| void * |
decryptContext,
|
||
| void * |
authContext,
|
||
| uint8_t |
flags
|
||
| ) |
Initialize the parser's context
- Parameters
-
contextPointer to context for the parser implementation decryptContextPointer to context for decryption of parsed file authContextPointer to context for authentication of parsed file flagsFlags for parser support
- Returns
- BOOTLOADER_OK if OK, error code otherwise.
| int32_t parser_parse | ( | void * |
context,
|
| ImageProperties_t * |
imageProperties,
|
||
| uint8_t |
buffer[],
|
||
| size_t |
length,
|
||
| const BootloaderParserCallbacks_t * |
callbacks
|
||
| ) |
Parse an image file in order to extract the binary and some metadata.
Pushes data into the image file parser to be parsed.
- Parameters
-
contextPointer to the specific parser's context variable imagePropertiesPointer to the image file state variable bufferPointer to byte array containing data to parse lengthSize in bytes of the data in buffer callbacksStruct containing function pointers to be called by the parser to pass the extracted binary data back to BTL.
- Returns
- BOOTLOADER_OK if OK, error code otherwise.
| bool parser_requireAuthenticity | ( | void |
|
) |
Check whether the parser requires images to be signed
- Returns
- True if authenticity is required, else false
| bool parser_requireConfidentiality | ( | void |
|
) |
Check whether the parser requires images to be encrypted
- Returns
- True if confidentiality is required, else false
| uint32_t parser_getApplicationAddress | ( | void |
|
) |
Return the start address of the application
- Returns
- start address of the application
| uint32_t parser_getBootloaderUpgradeAddress | ( | void |
|
) |
Return the start address of the bootloader upgrade location
- Returns
- start address of the bootloader upgrade location if upgrading is supported, otherwise 0.
| bool parser_applicationUpgradeValidCallback | ( | ApplicationData_t * |
app
|
) |
Callback to tell the parser whether to accept the application upgrade present in the upgrade image.
- Parameters
-
[in] appPointer to the application data structure contained in the upgrade image.
- Returns
- True if the application is accepted, and the parser should continue. False if the application is rejected. If rejected, the parser will abort parsing the image file and return BOOTLOADER_ERROR_PARSER_REJECTED .