EblEncryptionHeader_t Struct ReferencePlugin > Image Parser > GBL Parser > GBL Format
Description
GBL encryption header tag type.
Definition at line 92
of file btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields | |
EblTagHeader_t | header |
Tag ID and length. | |
uint32_t | version |
Version of the GBL spec used in this file. | |
uint32_t | magicWord |
Magic word (GBL_IMAGE_MAGIC_WORD) | |
uint32_t | encryptionType |
Type of encryption used. 1 = AES-CTR. | |
The documentation for this struct was generated from the following file:
btl_gbl_format.h