BootloaderParserContext Struct Reference
Description
Context used by bootloader image parser to store parser state.
Definition at line 24
of file btl_parse.h
.
#include <
btl_parse.h
>
Data Fields | |
ImageProperties_t | imageProperties |
Properties of the image being parsed. | |
ParserContext_t | parserContext |
Context information for the image parser. | |
DecryptContext_t | decryptContext |
Decryption context information for the image parser. | |
AuthContext_t | authContext |
Authentication context information for the image parser. | |
uint32_t | slotId |
Slot ID to try and parse an image from. | |
uint32_t | slotSize |
Size of storage slot. | |
uint32_t | slotOffset |
Offset into storage slot. | |
int32_t | errorCode |
Error code returned by the image parser. | |
The documentation for this struct was generated from the following file:
btl_parse.h