tempdrv.c File Reference
TEMPDRV API implementation.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
       Definition in file
       
        tempdrv.c
       
       .
      
       #include "em_device.h"
      
      
       #include "
       
        em_system.h
       
       "
      
      
       #include "
       
        em_emu.h
       
       "
      
      
       #include "string.h"
      
      
       #include "
       
        tempdrv.h
       
       "
      
      
| Data Structures | |
| struct | TEMPDRV_CallbackSet_t | 
| Functions | |
| static Ecode_t | addCallback ( TEMPDRV_CallbackSet_t *set, int8_t temp, TEMPDRV_Callback_t callback) | 
| Attempt to add a callback to a set. | |
| static void | calibration (void) | 
| Prepare calibration values for temperature conversion. | |
| static bool | checkForDuplicates ( TEMPDRV_CallbackSet_t *set, int8_t temp) | 
| Check if another callback has registered the same temperature. | |
| static uint32_t | convertToEmu (int temp) | 
| Convert a temperature in °C to an EMU sensor value. | |
| static int | convertToTemp (uint32_t emu) | 
| Convert EMU value to degrees Celsius. | |
| static void | disableInterrupts (void) | 
| Turn off and clear EMU temperature related interrupts. | |
| void | EMU_IRQHandler (void) | 
| EMU Interrupt Handler. | |
| static int8_t | findCallbackSpace ( TEMPDRV_CallbackSet_t *set) | 
| Find an empty spot for callback in set. | |
| static bool | removeCallback ( TEMPDRV_CallbackSet_t *set, TEMPDRV_Callback_t callback) | 
| Remove a callback from the set. | |
| Ecode_t | TEMPDRV_DeInit (void) | 
| De-initialize the TEMP driver. | |
| Ecode_t | TEMPDRV_Enable (bool enable) | 
| Enable or disable the TEMP driver. | |
| uint8_t | TEMPDRV_GetActiveCallbacks ( TEMPDRV_LimitType_t limit) | 
| Get the number of active callbacks for a limit. | |
| int8_t | TEMPDRV_GetTemp (void) | 
| Get the current temperature. | |
| Ecode_t | TEMPDRV_Init (void) | 
| Initialize the TEMP driver. | |
| void | TEMPDRV_IRQHandler (void) | 
| TEMPDRV Interrupt Handler. | |
| Ecode_t | TEMPDRV_RegisterCallback (int8_t temp, TEMPDRV_LimitType_t limit, TEMPDRV_Callback_t callback) | 
| Register a callback in the TEMP driver. | |
| Ecode_t | TEMPDRV_UnregisterCallback ( TEMPDRV_Callback_t callback) | 
| Unregister a callback in the TEMP driver. | |
| static void | updateInterrupts (void) | 
| Update interrupts based on active callbacks. | |
| Variables | |
| static int | calibrationEMU | 
| static int | calibrationTEMP | 
| static uint8_t | fallbackEMU = 0x90 | 
| static uint8_t | fallbackTEMP = 25 | 
| static TEMPDRV_CallbackSet_t * | highCallback | 
| static TEMPDRV_CallbackSet_t * | lowCallback | 
| static TEMPDRV_CallbackSet_t | nullCallback = { NULL, 0 } | 
| static bool | TEMPDRV_EnableState = false | 
| static bool | TEMPDRV_InitState = false | 
| static TEMPDRV_CallbackSet_t | tempdrvHighCallbacks [TEMPDRV_CALLBACK_DEPTH] | 
| static TEMPDRV_CallbackSet_t | tempdrvLowCallbacks [TEMPDRV_CALLBACK_DEPTH] | 
Function Documentation
| 
 | static | 
Attempt to add a callback to a set.
- Parameters
- 
         [in] setCallback set to add callback to [in] tempTemperature to register callback at [in] callbackCallback function 
- Returns
- 
         - ECODE_EMDRV_TEMPDRV_OK on success.
- ECODE_EMDRV_TEMPDRV_NO_SPACE if there is no space left for callbacks.
 
        Definition at line
        
         293
        
        of file
        
         tempdrv.c
        
        .
       
References TEMPDRV_CallbackSet_t::callback , convertToEmu() , ECODE_EMDRV_TEMPDRV_NO_SPACE , ECODE_EMDRV_TEMPDRV_OK , findCallbackSpace() , TEMPDRV_CallbackSet_t::temp , and updateInterrupts() .
Referenced by TEMPDRV_RegisterCallback() .
| 
 | static | 
Check if another callback has registered the same temperature.
- Parameters
- 
         [in] setCallback set to search [in] tempTemperature to match 
- Returns
- 
         trueif a duplicate is found,falseif no duplicates is found.
        Definition at line
        
         349
        
        of file
        
         tempdrv.c
        
        .
       
References convertToEmu() .
Referenced by TEMPDRV_RegisterCallback() .
| 
 | static | 
Convert a temperature in °C to an EMU sensor value.
- Parameters
- 
         [in] tempTemperature to convert in degrees Celsius 
- Returns
- EMU temperature sensor value that represents the given temperature
        Definition at line
        
         403
        
        of file
        
         tempdrv.c
        
        .
       
Referenced by addCallback() , and checkForDuplicates() .
| 
 | static | 
Convert EMU value to degrees Celsius.
- Parameters
- 
         [in] emuEMU value to convert 
- Returns
- temperature in degrees Celsius
        Definition at line
        
         376
        
        of file
        
         tempdrv.c
        
        .
       
Referenced by TEMPDRV_GetTemp() .
| 
 | static | 
Find an empty spot for callback in set.
- Parameters
- 
         [in] setCallback set to search 
- Returns
- index of empty space if found, -1 if none
        Definition at line
        
         263
        
        of file
        
         tempdrv.c
        
        .
       
Referenced by addCallback() .
| 
 | static | 
Remove a callback from the set.
- Parameters
- 
         [in] setCallback set to remove callback from [in] callbackCallback function 
- Returns
- 
         trueon success andfalseif the callback was not found.
        Definition at line
        
         320
        
        of file
        
         tempdrv.c
        
        .
       
References TEMPDRV_CallbackSet_t::callback , TEMPDRV_CallbackSet_t::temp , and updateInterrupts() .
Referenced by TEMPDRV_UnregisterCallback() .
| 
 | static | 
Update interrupts based on active callbacks.
There can only be two temperature thresholds active in the EMU sensor at a single point in time. One threshold for increasing temperature and one threshold for decreasing temperature. The responsibility of this function is to always select which temperature thresholds that should be activated in the EMU sensor at any given time.
        Definition at line
        
         440
        
        of file
        
         tempdrv.c
        
        .
       
References TEMPDRV_CallbackSet_t::callback , EMU_IntDisable() , EMU_IntEnable() , and TEMPDRV_CallbackSet_t::temp .
Referenced by addCallback() , removeCallback() , TEMPDRV_Enable() , TEMPDRV_Init() , and TEMPDRV_IRQHandler() .