Backbone Router

This module includes functions for the OpenThread Backbone Router Service.

Classes

struct otBackboneRouterConfig
This structure represents Backbone Router configuration.

Typedefs

typedef struct otBackboneRouterConfig otBackboneRouterConfig
This structure represents Backbone Router configuration.

Enumerations

enum otBackboneRouterState {
OT_BACKBONE_ROUTER_STATE_DISABLED = 0,
OT_BACKBONE_ROUTER_STATE_SECONDARY = 1,
OT_BACKBONE_ROUTER_STATE_PRIMARY = 2
}
Represents the Backbone Router Status.

Functions

otError otBackboneRouterGetPrimary ( otInstance *aInstance, otBackboneRouterConfig *aConfig)
This function gets the Primary Backbone Router information in the Thread Network.
void otBackboneRouterSetEnabled ( otInstance *aInstance, bool aEnable)
This function enables or disables Backbone functionality.
otBackboneRouterState otBackboneRouterGetState ( otInstance *aInstance)
This function gets the Backbone Router state.
void otBackboneRouterGetConfig ( otInstance *aInstance, otBackboneRouterConfig *aConfig)
This function gets the local Backbone Router configuration.
void otBackboneRouterSetConfig ( otInstance *aInstance, const otBackboneRouterConfig *aConfig)
This function sets the local Backbone Router configuration.
otError otBackboneRouterRegister ( otInstance *aInstance)
This function explicitly registers local Backbone Router configuration.
uint8_t otBackboneRouterGetRegistrationJitter ( otInstance *aInstance)
This method returns the Backbone Router registration jitter value.
void otBackboneRouterSetRegistrationJitter ( otInstance *aInstance, uint8_t aJitter)
This method sets the Backbone Router registration jitter value.
otError otBackboneRouterGetDomainPrefix ( otInstance *aInstance, otBorderRouterConfig *aConfig)
This method gets the local Domain Prefix configuration.

Detailed Description

This module includes functions for the OpenThread Backbone Router Service.

Enumeration Type Documentation

◆ otBackboneRouterState

Represents the Backbone Router Status.

Enumerator
OT_BACKBONE_ROUTER_STATE_DISABLED

Backbone function is disabled.

OT_BACKBONE_ROUTER_STATE_SECONDARY

Secondary Backbone Router.

OT_BACKBONE_ROUTER_STATE_PRIMARY

The Primary Backbone Router.

Function Documentation

◆ otBackboneRouterGetConfig()

void otBackboneRouterGetConfig ( otInstance * aInstance,
otBackboneRouterConfig * aConfig
)

This function gets the local Backbone Router configuration.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aConfig A pointer where to put local Backbone Router configuration.
See also
otBackboneRouterSetEnabled
otBackboneRouterGetState
otBackboneRouterSetConfig
otBackboneRouterRegister

◆ otBackboneRouterGetDomainPrefix()

otError otBackboneRouterGetDomainPrefix ( otInstance * aInstance,
otBorderRouterConfig * aConfig
)

This method gets the local Domain Prefix configuration.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aConfig A pointer to the Domain Prefix configuration.
Return values
OT_ERROR_NONE Successfully got the Domain Prefix configuration.
OT_ERROR_NOT_FOUND No Domain Prefix was configured.

◆ otBackboneRouterGetPrimary()

otError otBackboneRouterGetPrimary ( otInstance * aInstance,
otBackboneRouterConfig * aConfig
)

This function gets the Primary Backbone Router information in the Thread Network.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aConfig A pointer to where to put Primary Backbone Router information.
Return values
OT_ERROR_NONE Successfully got Primary Backbone Router information.
OT_ERROR_NOT_FOUND No Primary Backbone Router exists.

◆ otBackboneRouterGetRegistrationJitter()

uint8_t otBackboneRouterGetRegistrationJitter ( otInstance * aInstance )

This method returns the Backbone Router registration jitter value.

Returns
The Backbone Router registration jitter value.
See also
otBackboneRouterSetRegistrationJitter

◆ otBackboneRouterGetState()

otBackboneRouterState otBackboneRouterGetState ( otInstance * aInstance )

This function gets the Backbone Router state.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_BACKBONE_ROUTER_STATE_DISABLED Backbone functionality is disabled.
OT_BACKBONE_ROUTER_STATE_SECONDARY Secondary Backbone Router.
OT_BACKBONE_ROUTER_STATE_PRIMARY The Primary Backbone Router.
See also
otBackboneRouterSetEnabled
otBackboneRouterGetConfig
otBackboneRouterSetConfig
otBackboneRouterRegister

◆ otBackboneRouterRegister()

otError otBackboneRouterRegister ( otInstance * aInstance )

This function explicitly registers local Backbone Router configuration.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NO_BUFS Insufficient space to add the Backbone Router service.
OT_ERROR_NONE Successfully queued a Server Data Request message for delivery.
See also
otBackboneRouterSetEnabled
otBackboneRouterGetState
otBackboneRouterGetConfig
otBackboneRouterSetConfig

◆ otBackboneRouterSetConfig()

void otBackboneRouterSetConfig ( otInstance * aInstance,
const otBackboneRouterConfig * aConfig
)

This function sets the local Backbone Router configuration.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aConfig A pointer to the Backbone Router configuration to take effect.
See also
otBackboneRouterSetEnabled
otBackboneRouterGetState
otBackboneRouterGetConfig
otBackboneRouterRegister

◆ otBackboneRouterSetEnabled()

void otBackboneRouterSetEnabled ( otInstance * aInstance,
bool aEnable
)

This function enables or disables Backbone functionality.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aEnable TRUE to enable Backbone functionality, FALSE otherwise.
See also
otBackboneRouterGetState
otBackboneRouterGetConfig
otBackboneRouterSetConfig
otBackboneRouterRegister

◆ otBackboneRouterSetRegistrationJitter()

void otBackboneRouterSetRegistrationJitter ( otInstance * aInstance,
uint8_t aJitter
)

This method sets the Backbone Router registration jitter value.

Parameters
[in] aJitter the Backbone Router registration jitter value to set.
See also
otBackboneRouterGetRegistrationJitter