otRadioCoexMetrics Struct Reference
The following are valid radio state transitions:
#include <
include/openthread/platform/radio.h
>
Public Attributes | |
uint32_t | mNumGrantGlitch |
Number of grant glitches. | |
uint32_t | mNumTxRequest |
Number of tx requests. | |
uint32_t | mNumTxGrantImmediate |
Number of tx requests while grant was active. | |
uint32_t | mNumTxGrantWait |
Number of tx requests while grant was inactive. | |
uint32_t | mNumTxGrantWaitActivated |
Number of tx requests while grant was inactive that were ultimately granted. | |
uint32_t | mNumTxGrantWaitTimeout |
Number of tx requests while grant was inactive that timed out. | |
uint32_t | mNumTxGrantDeactivatedDuringRequest |
Number of tx that were in progress when grant was deactivated. | |
uint32_t | mNumTxDelayedGrant |
Number of tx requests that were not granted within 50us. | |
uint32_t | mAvgTxRequestToGrantTime |
Average time in usec from tx request to grant. | |
uint32_t | mNumRxRequest |
Number of rx requests. | |
uint32_t | mNumRxGrantImmediate |
Number of rx requests while grant was active. | |
uint32_t | mNumRxGrantWait |
Number of rx requests while grant was inactive. | |
uint32_t | mNumRxGrantWaitActivated |
Number of rx requests while grant was inactive that were ultimately granted. | |
uint32_t | mNumRxGrantWaitTimeout |
Number of rx requests while grant was inactive that timed out. | |
uint32_t | mNumRxGrantDeactivatedDuringRequest |
Number of rx that were in progress when grant was deactivated. | |
uint32_t | mNumRxDelayedGrant |
Number of rx requests that were not granted within 50us. | |
uint32_t | mAvgRxRequestToGrantTime |
Average time in usec from rx request to grant. | |
uint32_t | mNumRxGrantNone |
Number of rx requests that completed without receiving grant. | |
bool | mStopped |
Stats collection stopped due to saturation. |
The following are valid radio state transitions:
(Radio ON) +----——+ Enable() +-——+ Receive() +---——+ Transmit() +----——+ | |-----——>| |-----——>| |--------——>| | | Disabled | | Sleep | | Receive | | Transmit | | |<-----——| |<-----——| |<--------——| | +----——+ Disable() +-——+ Sleep() +---——+ Receive() +----——+ (Radio OFF) or signal TransmitDone
During the IEEE 802.15.4 data request command the transition Sleep->Receive->Transmit can be shortened to direct transition from Sleep to Transmit if the platform supports the OT_RADIO_CAPS_SLEEP_TO_TX capability. This structure represents radio coexistence metrics.
The documentation for this struct was generated from the following file:
- include/openthread/platform/
radio.h