This module includes functions for Thread Routers and Leaders.
Classes | |
struct | otChildInfo |
This structure holds diagnostic information for a Thread Child. | |
struct | otCacheEntryInfo |
This structure represents an EID cache entry. | |
struct | otCacheEntryIterator |
This type represents an iterator used for iterating through the EID cache table entries. | |
struct | otNeighborTableEntryInfo |
This type represent a neighbor table entry info (child or router) and is used as a parameter in the neighbor table callback otNeighborTableCallback . |
Macros | |
#define | OT_CHILD_IP6_ADDRESS_ITERATOR_INIT 0 |
Initializer for otChildIP6AddressIterator. |
Typedefs | |
typedef uint16_t | otChildIp6AddressIterator |
Used to iterate through IPv6 addresses of a Thread Child entry. | |
typedef enum otCacheEntryState | otCacheEntryState |
This enumeration defines the EID cache entry state. | |
typedef struct otCacheEntryInfo | otCacheEntryInfo |
This structure represents an EID cache entry. | |
typedef struct otCacheEntryIterator | otCacheEntryIterator |
This type represents an iterator used for iterating through the EID cache table entries. | |
typedef void(* | otNeighborTableCallback) (otNeighborTableEvent aEvent, const otNeighborTableEntryInfo *aEntryInfo) |
This function pointer is called to notify that a child or router neighbor is being added to or removed from neighbor table. |
Enumerations | |
enum | otCacheEntryState { OT_CACHE_ENTRY_STATE_CACHED = 0, OT_CACHE_ENTRY_STATE_SNOOPED = 1, OT_CACHE_ENTRY_STATE_QUERY = 2, OT_CACHE_ENTRY_STATE_RETRY_QUERY = 3 } |
This enumeration defines the EID cache entry state. | |
enum | otNeighborTableEvent { OT_NEIGHBOR_TABLE_EVENT_CHILD_ADDED, OT_NEIGHBOR_TABLE_EVENT_CHILD_REMOVED, OT_NEIGHBOR_TABLE_EVENT_ROUTER_ADDED, OT_NEIGHBOR_TABLE_EVENT_ROUTER_REMOVED } |
This enumeration defines the constants used in otNeighborTableCallback to indicate whether a child or router neighbor is being added or removed. |
Functions | |
uint16_t | otThreadGetMaxAllowedChildren (otInstance *aInstance) |
Get the maximum number of children currently allowed. | |
otError | otThreadSetMaxAllowedChildren (otInstance *aInstance, uint16_t aMaxChildren) |
Set the maximum number of children currently allowed. | |
bool | otThreadIsRouterEligible (otInstance *aInstance) |
This method indicates whether or not the device is router-eligible. | |
otError | otThreadSetRouterEligible (otInstance *aInstance, bool aEligible) |
This function sets whether or not the device is router-eligible. | |
otError | otThreadSetPreferredRouterId (otInstance *aInstance, uint8_t aRouterId) |
Set the preferred Router Id. | |
uint8_t | otThreadGetLocalLeaderWeight (otInstance *aInstance) |
Get the Thread Leader Weight used when operating in the Leader role. | |
void | otThreadSetLocalLeaderWeight (otInstance *aInstance, uint8_t aWeight) |
Set the Thread Leader Weight used when operating in the Leader role. | |
uint32_t | otThreadGetLocalLeaderPartitionId (otInstance *aInstance) |
Get the Thread Leader Partition Id used when operating in the Leader role. | |
void | otThreadSetLocalLeaderPartitionId (otInstance *aInstance, uint32_t aPartitionId) |
Set the Thread Leader Partition Id used when operating in the Leader role. | |
uint16_t | otThreadGetJoinerUdpPort (otInstance *aInstance) |
Get the Joiner UDP Port. | |
otError | otThreadSetJoinerUdpPort (otInstance *aInstance, uint16_t aJoinerUdpPort) |
Set the Joiner UDP Port. | |
void | otThreadSetSteeringData (otInstance *aInstance, const otExtAddress *aExtAddress) |
Set Steering data out of band. | |
uint32_t | otThreadGetContextIdReuseDelay (otInstance *aInstance) |
Get the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role. | |
void | otThreadSetContextIdReuseDelay (otInstance *aInstance, uint32_t aDelay) |
Set the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role. | |
uint8_t | otThreadGetNetworkIdTimeout (otInstance *aInstance) |
Get the NETWORK_ID_TIMEOUT parameter used in the Router role. | |
void | otThreadSetNetworkIdTimeout (otInstance *aInstance, uint8_t aTimeout) |
Set the NETWORK_ID_TIMEOUT parameter used in the Leader role. | |
uint8_t | otThreadGetRouterUpgradeThreshold (otInstance *aInstance) |
Get the ROUTER_UPGRADE_THRESHOLD parameter used in the REED role. | |
void | otThreadSetRouterUpgradeThreshold (otInstance *aInstance, uint8_t aThreshold) |
Set the ROUTER_UPGRADE_THRESHOLD parameter used in the Leader role. | |
otError | otThreadReleaseRouterId (otInstance *aInstance, uint8_t aRouterId) |
Release a Router ID that has been allocated by the device in the Leader role. | |
otError | otThreadBecomeRouter (otInstance *aInstance) |
Attempt to become a router. | |
otError | otThreadBecomeLeader (otInstance *aInstance) |
Become a leader and start a new partition. | |
uint8_t | otThreadGetRouterDowngradeThreshold (otInstance *aInstance) |
Get the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Router role. | |
void | otThreadSetRouterDowngradeThreshold (otInstance *aInstance, uint8_t aThreshold) |
Set the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Leader role. | |
uint8_t | otThreadGetRouterSelectionJitter (otInstance *aInstance) |
Get the ROUTER_SELECTION_JITTER parameter used in the REED/Router role. | |
void | otThreadSetRouterSelectionJitter (otInstance *aInstance, uint8_t aRouterJitter) |
Set the ROUTER_SELECTION_JITTER parameter used in the REED/Router role. | |
otError | otThreadGetChildInfoById (otInstance *aInstance, uint16_t aChildId, otChildInfo *aChildInfo) |
The function retains diagnostic information for an attached Child by its Child ID or RLOC16. | |
otError | otThreadGetChildInfoByIndex (otInstance *aInstance, uint16_t aChildIndex, otChildInfo *aChildInfo) |
The function retains diagnostic information for an attached Child by the internal table index. | |
otError | otThreadGetChildNextIp6Address (otInstance *aInstance, uint16_t aChildIndex, otChildIp6AddressIterator *aIterator, otIp6Address *aAddress) |
This function gets the next IPv6 address (using an iterator) for a given child. | |
uint8_t | otThreadGetRouterIdSequence (otInstance *aInstance) |
Get the current Router ID Sequence. | |
uint8_t | otThreadGetMaxRouterId (otInstance *aInstance) |
The function returns the maximum allowed router ID. | |
otError | otThreadGetRouterInfo (otInstance *aInstance, uint16_t aRouterId, otRouterInfo *aRouterInfo) |
The function retains diagnostic information for a given Thread Router. | |
otError | otThreadGetNextCacheEntry (otInstance *aInstance, otCacheEntryInfo *aEntryInfo, otCacheEntryIterator *aIterator) |
This function gets the next EID cache entry (using an iterator). | |
const otPskc * | otThreadGetPskc (otInstance *aInstance) |
Get the Thread PSKc. | |
otError | otThreadSetPskc (otInstance *aInstance, const otPskc *aPskc) |
Set the Thread PSKc. | |
int8_t | otThreadGetParentPriority (otInstance *aInstance) |
Get the assigned parent priority. | |
otError | otThreadSetParentPriority (otInstance *aInstance, int8_t aParentPriority) |
Set the parent priority. | |
uint8_t | otThreadGetMaxChildIpAddresses (otInstance *aInstance) |
This function gets the maximum number of IP addresses that each MTD child may register with this device as parent. | |
otError | otThreadSetMaxChildIpAddresses (otInstance *aInstance, uint8_t aMaxIpAddresses) |
This function sets/restores the maximum number of IP addresses that each MTD child may register with this device as parent. | |
void | otThreadRegisterNeighborTableCallback (otInstance *aInstance, otNeighborTableCallback aCallback) |
This function registers a neighbor table callback function. |
Detailed Description
This module includes functions for Thread Routers and Leaders.
Typedef Documentation
◆ otCacheEntryIterator
typedef struct otCacheEntryIterator otCacheEntryIterator |
This type represents an iterator used for iterating through the EID cache table entries.
To initialize the iterator and start from the first entry in the cache table, set all its fields in the structure to zero (e.g., memset
the iterator to zero).
◆ otNeighborTableCallback
typedef void(* otNeighborTableCallback) (otNeighborTableEvent aEvent, const otNeighborTableEntryInfo *aEntryInfo) |
This function pointer is called to notify that a child or router neighbor is being added to or removed from neighbor table.
- Parameters
-
[in] aEvent
A event flag. [in] aEntryInfo
A pointer to table entry info.
Enumeration Type Documentation
◆ otNeighborTableEvent
enum otNeighborTableEvent |
This enumeration defines the constants used in otNeighborTableCallback
to indicate whether a child or router neighbor is being added or removed.
Function Documentation
◆ otThreadBecomeLeader()
otError otThreadBecomeLeader | ( | otInstance * | aInstance | ) |
Become a leader and start a new partition.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONE
Successfully became a leader and started a new partition. OT_ERROR_INVALID_STATE
Thread is disabled.
◆ otThreadBecomeRouter()
otError otThreadBecomeRouter | ( | otInstance * | aInstance | ) |
Attempt to become a router.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONE
Successfully begin attempt to become a router. OT_ERROR_INVALID_STATE
Thread is disabled.
◆ otThreadGetChildInfoById()
otError otThreadGetChildInfoById | ( | otInstance * | aInstance, |
uint16_t | aChildId, |
||
otChildInfo * | aChildInfo |
||
) |
The function retains diagnostic information for an attached Child by its Child ID or RLOC16.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aChildId
The Child ID or RLOC16 for the attached child. [out] aChildInfo
A pointer to where the child information is placed.
- Return values
-
OT_ERROR_NONE
aChildInfo
was successfully updated with the info for the given ID.OT_ERROR_NOT_FOUND
No valid child with this Child ID. OT_ERROR_INVALID_ARGS
If aChildInfo
is NULL.
◆ otThreadGetChildInfoByIndex()
otError otThreadGetChildInfoByIndex | ( | otInstance * | aInstance, |
uint16_t | aChildIndex, |
||
otChildInfo * | aChildInfo |
||
) |
The function retains diagnostic information for an attached Child by the internal table index.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aChildIndex
The table index. [out] aChildInfo
A pointer to where the child information is placed.
- Return values
-
OT_ERROR_NONE
aChildInfo
was successfully updated with the info for the given index.OT_ERROR_NOT_FOUND
No valid child at this index. OT_ERROR_INVALID_ARGS
Either aChildInfo
is NULL, oraChildIndex
is out of range (higher than max table index).
- See also
- otGetMaxAllowedChildren
◆ otThreadGetChildNextIp6Address()
otError otThreadGetChildNextIp6Address | ( | otInstance * | aInstance, |
uint16_t | aChildIndex, |
||
otChildIp6AddressIterator * | aIterator, |
||
otIp6Address * | aAddress |
||
) |
This function gets the next IPv6 address (using an iterator) for a given child.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aChildIndex
The child index. [in,out] aIterator
A pointer to the iterator. On success the iterator will be updated to point to next entry in the list. To get the first IPv6 address the iterator should be set to OT_CHILD_IP6_ADDRESS_ITERATOR_INIT. [out] aAddress
A pointer to an IPv6 address where the child's next address is placed (on success).
- Return values
-
OT_ERROR_NONE
Successfully found the next IPv6 address ( aAddress
was successfully updated).OT_ERROR_NOT_FOUND
The child has no subsequent IPv6 address entry. OT_ERROR_INVALID_ARGS
aIterator
oraAddress
are NULL, or child ataChildIndex
is not valid.
- See also
- otThreadGetChildInfoByIndex
◆ otThreadGetContextIdReuseDelay()
uint32_t otThreadGetContextIdReuseDelay | ( | otInstance * | aInstance | ) |
Get the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The CONTEXT_ID_REUSE_DELAY value.
- See also
- otThreadSetContextIdReuseDelay
◆ otThreadGetJoinerUdpPort()
uint16_t otThreadGetJoinerUdpPort | ( | otInstance * | aInstance | ) |
Get the Joiner UDP Port.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Joiner UDP Port number.
- See also
- otThreadSetJoinerUdpPort
◆ otThreadGetLocalLeaderPartitionId()
uint32_t otThreadGetLocalLeaderPartitionId | ( | otInstance * | aInstance | ) |
Get the Thread Leader Partition Id used when operating in the Leader role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Thread Leader Partition Id value.
◆ otThreadGetLocalLeaderWeight()
uint8_t otThreadGetLocalLeaderWeight | ( | otInstance * | aInstance | ) |
Get the Thread Leader Weight used when operating in the Leader role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Thread Leader Weight value.
- See also
- otThreadSetLeaderWeight
◆ otThreadGetMaxAllowedChildren()
uint16_t otThreadGetMaxAllowedChildren | ( | otInstance * | aInstance | ) |
Get the maximum number of children currently allowed.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The maximum number of children currently allowed.
- See also
- otThreadSetMaxAllowedChildren
◆ otThreadGetMaxChildIpAddresses()
uint8_t otThreadGetMaxChildIpAddresses | ( | otInstance * | aInstance | ) |
This function gets the maximum number of IP addresses that each MTD child may register with this device as parent.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The maximum number of IP addresses that each MTD child may register with this device as parent.
- See also
- otThreadSetMaxChildIpAddresses
◆ otThreadGetMaxRouterId()
uint8_t otThreadGetMaxRouterId | ( | otInstance * | aInstance | ) |
The function returns the maximum allowed router ID.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The maximum allowed router ID.
◆ otThreadGetNetworkIdTimeout()
uint8_t otThreadGetNetworkIdTimeout | ( | otInstance * | aInstance | ) |
Get the NETWORK_ID_TIMEOUT parameter used in the Router role.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The NETWORK_ID_TIMEOUT value.
- See also
- otThreadSetNetworkIdTimeout
◆ otThreadGetNextCacheEntry()
otError otThreadGetNextCacheEntry | ( | otInstance * | aInstance, |
otCacheEntryInfo * | aEntryInfo, |
||
otCacheEntryIterator * | aIterator |
||
) |
This function gets the next EID cache entry (using an iterator).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [out] aEntryInfo
A pointer to where the EID cache entry information is placed. [in,out] aIterator
A pointer to an iterator. It will be updated to point to next entry on success. To get the first entry, initialize the iterator by setting all its fields to zero (e.g., memset
the the iterator structure to zero).
- Return values
-
OT_ERROR_NONE
Successfully populated aEntryInfo
for next EID cache entry.OT_ERROR_NOT_FOUND
No more entries in the address cache table.
◆ otThreadGetParentPriority()
int8_t otThreadGetParentPriority | ( | otInstance * | aInstance | ) |
Get the assigned parent priority.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The assigned parent priority value, -2 means not assigned.
- See also
- otThreadSetParentPriority
◆ otThreadGetPskc()
const otPskc* otThreadGetPskc | ( | otInstance * | aInstance | ) |
Get the Thread PSKc.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- A pointer to Thread PSKc
- See also
- otThreadSetPskc
◆ otThreadGetRouterDowngradeThreshold()
uint8_t otThreadGetRouterDowngradeThreshold | ( | otInstance * | aInstance | ) |
Get the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Router role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The ROUTER_DOWNGRADE_THRESHOLD value.
◆ otThreadGetRouterIdSequence()
uint8_t otThreadGetRouterIdSequence | ( | otInstance * | aInstance | ) |
Get the current Router ID Sequence.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Router ID Sequence.
◆ otThreadGetRouterInfo()
otError otThreadGetRouterInfo | ( | otInstance * | aInstance, |
uint16_t | aRouterId, |
||
otRouterInfo * | aRouterInfo |
||
) |
The function retains diagnostic information for a given Thread Router.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRouterId
The router ID or RLOC16 for a given router. [out] aRouterInfo
A pointer to where the router information is placed.
- Return values
-
OT_ERROR_NONE
Successfully retrieved the router info for given id. OT_ERROR_NOT_FOUND
No router entry with the given id. OT_ERROR_INVALID_ARGS
aRouterInfo
is NULL.
◆ otThreadGetRouterSelectionJitter()
uint8_t otThreadGetRouterSelectionJitter | ( | otInstance * | aInstance | ) |
Get the ROUTER_SELECTION_JITTER parameter used in the REED/Router role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The ROUTER_SELECTION_JITTER value.
- See also
- otThreadSetRouterSelectionJitter
◆ otThreadGetRouterUpgradeThreshold()
uint8_t otThreadGetRouterUpgradeThreshold | ( | otInstance * | aInstance | ) |
Get the ROUTER_UPGRADE_THRESHOLD parameter used in the REED role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The ROUTER_UPGRADE_THRESHOLD value.
◆ otThreadIsRouterEligible()
bool otThreadIsRouterEligible | ( | otInstance * | aInstance | ) |
This method indicates whether or not the device is router-eligible.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
TRUE
If device is router-eligible. FALSE
If device is not router-eligible.
◆ otThreadRegisterNeighborTableCallback()
void otThreadRegisterNeighborTableCallback | ( | otInstance * | aInstance, |
otNeighborTableCallback | aCallback |
||
) |
This function registers a neighbor table callback function.
The provided callback (if non-NULL) will be invoked when a child or router neighbor entry is being added/removed to/from the neighbor table. Subsequent calls to this method will overwrite the previous callback. Note that this callback in invoked while the neighbor/child table is being updated and always before the otStateChangedCallback
.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aCallback
A pointer to callback handler function.
◆ otThreadReleaseRouterId()
otError otThreadReleaseRouterId | ( | otInstance * | aInstance, |
uint8_t | aRouterId |
||
) |
Release a Router ID that has been allocated by the device in the Leader role.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRouterId
The Router ID to release. Valid range is [0, 62].
- Return values
-
OT_ERROR_NONE
Successfully released the router id. OT_ERROR_INVALID_ARGS
aRouterId
is not in the range [0, 62].OT_ERROR_INVALID_STATE
The device is not currently operating as a leader. OT_ERROR_NOT_FOUND
The router id is not currently allocated.
◆ otThreadSetContextIdReuseDelay()
void otThreadSetContextIdReuseDelay | ( | otInstance * | aInstance, |
uint32_t | aDelay |
||
) |
Set the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aDelay
The CONTEXT_ID_REUSE_DELAY value.
- See also
- otThreadGetContextIdReuseDelay
◆ otThreadSetJoinerUdpPort()
otError otThreadSetJoinerUdpPort | ( | otInstance * | aInstance, |
uint16_t | aJoinerUdpPort |
||
) |
Set the Joiner UDP Port.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aJoinerUdpPort
The Joiner UDP Port number.
- Return values
-
OT_ERROR_NONE
Successfully set the Joiner UDP Port.
- See also
- otThreadGetJoinerUdpPort
◆ otThreadSetLocalLeaderPartitionId()
void otThreadSetLocalLeaderPartitionId | ( | otInstance * | aInstance, |
uint32_t | aPartitionId |
||
) |
Set the Thread Leader Partition Id used when operating in the Leader role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPartitionId
The Thread Leader Partition Id value.
◆ otThreadSetLocalLeaderWeight()
void otThreadSetLocalLeaderWeight | ( | otInstance * | aInstance, |
uint8_t | aWeight |
||
) |
Set the Thread Leader Weight used when operating in the Leader role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aWeight
The Thread Leader Weight value.
- See also
- otThreadGetLeaderWeight
◆ otThreadSetMaxAllowedChildren()
otError otThreadSetMaxAllowedChildren | ( | otInstance * | aInstance, |
uint16_t | aMaxChildren |
||
) |
Set the maximum number of children currently allowed.
This parameter can only be set when Thread protocol operation has been stopped.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMaxChildren
The maximum allowed children.
- Return values
-
OT_ERROR_NONE
Successfully set the max. OT_ERROR_INVALID_ARGS
If aMaxChildren
is not in the range [1, OPENTHREAD_CONFIG_MLE_MAX_CHILDREN].OT_ERROR_INVALID_STATE
If Thread isn't stopped.
- See also
- otThreadGetMaxAllowedChildren
◆ otThreadSetMaxChildIpAddresses()
otError otThreadSetMaxChildIpAddresses | ( | otInstance * | aInstance, |
uint8_t | aMaxIpAddresses |
||
) |
This function sets/restores the maximum number of IP addresses that each MTD child may register with this device as parent.
- Note
- This API requires
OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
, and is only used by Thread Test Harness to limit the address registrations of the reference parent in order to test the MTD DUT reaction.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMaxIpAddresses
The maximum number of IP addresses that each MTD child may register with this device as parent. 0 to clear the setting and restore the default.
- Return values
-
OT_ERROR_NONE
Successfully set/cleared the number. OT_ERROR_INVALID_ARGS
If exceeds the allowed maximum number.
- See also
- otThreadGetMaxChildIpAddresses
◆ otThreadSetNetworkIdTimeout()
void otThreadSetNetworkIdTimeout | ( | otInstance * | aInstance, |
uint8_t | aTimeout |
||
) |
Set the NETWORK_ID_TIMEOUT parameter used in the Leader role.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aTimeout
The NETWORK_ID_TIMEOUT value.
- See also
- otThreadGetNetworkIdTimeout
◆ otThreadSetParentPriority()
otError otThreadSetParentPriority | ( | otInstance * | aInstance, |
int8_t | aParentPriority |
||
) |
Set the parent priority.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aParentPriority
The parent priority value.
- Return values
-
OT_ERROR_NONE
Successfully set the parent priority. OT_ERROR_INVALID_ARGS
If the parent priority value is not among 1, 0, -1 and -2.
- See also
- otThreadGetParentPriority
◆ otThreadSetPreferredRouterId()
otError otThreadSetPreferredRouterId | ( | otInstance * | aInstance, |
uint8_t | aRouterId |
||
) |
Set the preferred Router Id.
Upon becoming a router/leader the node attempts to use this Router Id. If the preferred Router Id is not set or if it can not be used, a randomly generated router id is picked. This property can be set only when the device role is either detached or disabled.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRouterId
The preferred Router Id.
- Return values
-
OT_ERROR_NONE
Successfully set the preferred Router Id. OT_ERROR_INVALID_STATE
Could not set (role is not detached or disabled)
◆ otThreadSetPskc()
otError otThreadSetPskc | ( | otInstance * | aInstance, |
const otPskc * | aPskc |
||
) |
Set the Thread PSKc.
This function will only succeed when Thread protocols are disabled. A successful call to this function will also invalidate the Active and Pending Operational Datasets in non-volatile memory.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPskc
A pointer to the new Thread PSKc.
- Return values
-
OT_ERROR_NONE
Successfully set the Thread PSKc. OT_ERROR_INVALID_STATE
Thread protocols are enabled.
- See also
- otThreadGetPskc
◆ otThreadSetRouterDowngradeThreshold()
void otThreadSetRouterDowngradeThreshold | ( | otInstance * | aInstance, |
uint8_t | aThreshold |
||
) |
Set the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Leader role.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aThreshold
The ROUTER_DOWNGRADE_THRESHOLD value.
◆ otThreadSetRouterEligible()
otError otThreadSetRouterEligible | ( | otInstance * | aInstance, |
bool | aEligible |
||
) |
This function sets whether or not the device is router-eligible.
If aEligible
is false and the device is currently operating as a router, this call will cause the device to detach and attempt to reattach as a child.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aEligible
TRUE to configure the device as router-eligible, FALSE otherwise.
- Return values
-
OT_ERROR_NONE
Successfully set the router-eligible configuration. OT_ERROR_NOT_CAPABLE
The device is not capable of becoming a router.
◆ otThreadSetRouterSelectionJitter()
void otThreadSetRouterSelectionJitter | ( | otInstance * | aInstance, |
uint8_t | aRouterJitter |
||
) |
Set the ROUTER_SELECTION_JITTER parameter used in the REED/Router role.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRouterJitter
The ROUTER_SELECTION_JITTER value.
- See also
- otThreadGetRouterSelectionJitter
◆ otThreadSetRouterUpgradeThreshold()
void otThreadSetRouterUpgradeThreshold | ( | otInstance * | aInstance, |
uint8_t | aThreshold |
||
) |
Set the ROUTER_UPGRADE_THRESHOLD parameter used in the Leader role.
- Note
- This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aThreshold
The ROUTER_UPGRADE_THRESHOLD value.
◆ otThreadSetSteeringData()
void otThreadSetSteeringData | ( | otInstance * | aInstance, |
const otExtAddress * | aExtAddress |
||
) |
Set Steering data out of band.
Configuration option OPENTHREAD_CONFIG_MLE_STEERING_DATA_SET_OOB_ENABLE
should be set to enable setting of steering data out of band.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aExtAddress
Address used to update the steering data. All zeros to clear the steering data (no steering data). All 0xFFs to set steering data/bloom filter to accept/allow all. A specific EUI64 which is then added to current steering data/bloom filter.