This module includes functions that control SNTP communication.
Classes | |
struct | otSntpQuery |
This structure implements SNTP Query parameters. |
Macros | |
#define | OT_SNTP_DEFAULT_SERVER_IP "2001:4860:4806:8::" |
Defines default SNTP Server address - Google NTP Server. | |
#define | OT_SNTP_DEFAULT_SERVER_PORT 123 |
Defines default SNTP Server port. |
Typedefs | |
typedef struct otSntpQuery | otSntpQuery |
This structure implements SNTP Query parameters. | |
typedef void(* | otSntpResponseHandler) (void *aContext, uint64_t aTime, otError aResult) |
This function pointer is called when a SNTP response is received. |
Functions | |
otError | otSntpClientQuery (otInstance *aInstance, const otSntpQuery *aQuery, otSntpResponseHandler aHandler, void *aContext) |
This function sends a SNTP query. | |
void | otSntpClientSetUnixEra (otInstance *aInstance, uint32_t aUnixEra) |
This function sets the unix era number. |
Detailed Description
This module includes functions that control SNTP communication.
Typedef Documentation
◆ otSntpResponseHandler
typedef void(* otSntpResponseHandler) (void *aContext, uint64_t aTime, otError aResult) |
This function pointer is called when a SNTP response is received.
- Parameters
-
[in] aContext
A pointer to application-specific context. [in] aTime
Specifies the time at the server when the response left for the client, in UNIX time. [in] aResult
A result of the SNTP transaction.
- Return values
-
OT_ERROR_NONE
A response was received successfully and time is provided in aTime
.OT_ERROR_ABORT
A SNTP transaction was aborted by stack. OT_ERROR_BUSY
The Kiss-o'-death packet has been received. OT_ERROR_RESPONSE_TIMEOUT
No SNTP response has been received within timeout. OT_ERROR_FAILED
A response was received but contains incorrect data.
Function Documentation
◆ otSntpClientQuery()
otError otSntpClientQuery | ( | otInstance * | aInstance, |
const otSntpQuery * | aQuery, |
||
otSntpResponseHandler | aHandler, |
||
void * | aContext |
||
) |
This function sends a SNTP query.
This function is available only if feature OPENTHREAD_CONFIG_SNTP_CLIENT_ENABLE_CLIENT
is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aQuery
A pointer to specify SNTP query parameters. [in] aHandler
A function pointer that shall be called on response reception or time-out. [in] aContext
A pointer to arbitrary context information.
◆ otSntpClientSetUnixEra()
void otSntpClientSetUnixEra | ( | otInstance * | aInstance, |
uint32_t | aUnixEra |
||
) |
This function sets the unix era number.
The default value of unix era is set to 0. The subsequent eras start after year 2106.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aUnixEra
Unix era number.