This module includes functions that control DNS communication.
|
struct | otDnsQuery |
| This structure implements DNS Query parameters.
|
This module includes functions that control DNS communication.
◆ otDnsResponseHandler
typedef void(* otDnsResponseHandler) (void *aContext, const char *aHostname, const otIp6Address *aAddress, uint32_t aTtl, otError aResult) |
This function pointer is called when a DNS response is received.
- Parameters
-
[in] | aContext | A pointer to application-specific context. |
[in] | aHostname | Identifies hostname related with DNS response. |
[in] | aAddress | A pointer to the IPv6 address received in DNS response. May be null. |
[in] | aTtl | Specifies the maximum time in seconds that the resource record may be cached. |
[in] | aResult | A result of the DNS transaction. |
- Return values
-
OT_ERROR_NONE | A response was received successfully and IPv6 address is provided in aAddress . |
OT_ERROR_ABORT | A DNS transaction was aborted by stack. |
OT_ERROR_RESPONSE_TIMEOUT | No DNS response has been received within timeout. |
OT_ERROR_NOT_FOUND | A response was received but no IPv6 address has been found. |
OT_ERROR_FAILED | A response was received but status code is different than success. |
◆ otDnsClientQuery()
This function sends a DNS query for AAAA (IPv6) record.
This function is available only if feature OPENTHREAD_CONFIG_DNS_CLIENT_ENABLE
is enabled.
- Parameters
-
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aQuery | A pointer to specify DNS query parameters. |
[in] | aHandler | A function pointer that shall be called on response reception or time-out. |
[in] | aContext | A pointer to arbitrary context information. |