This structure represents the MLE Parent Response data.
#include <
include/openthread/thread.h
>
Public Attributes | |
otExtAddress | mExtAddr |
IEEE 802.15.4 Extended Address of the Parent. | |
uint16_t | mRloc16 |
Short address of the Parent. | |
int8_t | mRssi |
Rssi of the Parent. | |
int8_t | mPriority |
Parent priority. | |
uint8_t | mLinkQuality3 |
Parent Link Quality 3. | |
uint8_t | mLinkQuality2 |
Parent Link Quality 2. | |
uint8_t | mLinkQuality1 |
Parent Link Quality 1. | |
bool | mIsAttached |
Is the node receiving parent response attached. |
This structure represents the MLE Parent Response data.
The documentation for this struct was generated from the following file:
- include/openthread/
thread.h